3.2.27 MLME_SetConf_t Struct
C
typedef struct mlme_set_conf_tag {
/** This identifies the message as \ref MLME_SET_CONFIRM */
enum msg_code cmdcode;
/** The result of the request to write the MAC PIB attribute. */
uint8_t status;
/** The identifier of the MAC PIB attribute that was written. */
uint8_t PIBAttribute;
#if ((defined MAC_SECURITY_ZIP) || (defined MAC_SECURITY_2006))
/** The index within the table of the specified MAC PIB attribute to set. */
uint8_t PIBAttributeIndex;
#endif
} MLME_SetConf_t;
Summary
MLME_SetConf_t holds the MLME-SET.confirm message structure
Description
None
Remarks
None