3.2.28 MLME_RxEnableReq_t Struct
C
typedef struct mlme_rx_enable_req_tag {
/** This identifies the message as \ref MLME_RX_ENABLE_REQUEST */
enum msg_code cmdcode;
/** TRUE if the receiver enable can be deferred until during the next
* superframe if the requested time has already passed. FALSE if the
* receiver enable is only to be attempted in the current superframe.
* This parameter is ignored for nonbeacon-enabled PANs. */
uint8_t DeferPermit;
/** The number of symbols from the start of the superframe before the
* receiver is to be enabled. The precision of this value is a minimum of
* 20 bits, with the lowest 4 bits being the least significant. This
* parameter is ignored for nonbeacon-enabled PANs. */
uint32_t RxOnTime;
/** The number of symbols for which the receiver is to be enabled. */
uint32_t RxOnDuration;
} MLME_RxEnableReq_t;
Summary
MLME_RxEnableReq_t holds the MLME-RX-ENABLE.request message structure
Description
None
Remarks
None