3.2.32 MLME_CommStatusInd_t Struct
C
typedef struct mlme_comm_status_ind_tag {
/** This identifies the message as \ref MLME_COMM_STATUS_INDICATION */
enum msg_code cmdcode;
/** The 16 bit PAN identifier of the device from which the frame was
* received or to which the frame was being sent. */
uint16_t PANId;
/** The source addressing mode for this primitive. This value can take one
* of the following values: 0 = no address (addressing fields omitted).
* 0 x 01 = reserved. 0 x 02 = 16 bit short address. 0 x 03 = 64 bit
* extended address. */
uint8_t SrcAddrMode;
/** The source addressing mode for this primitive. This value can take one
* of the following values: 0 = no address (addressing fields omitted).
* 0 x 01 = reserved. 0 x 02 = 16 bit short address. 0 x 03 = 64 bit
* extended address. */
uint64_t SrcAddr;
/** The destination addressing mode for this primitive. This value can take
* one of the following values: 0 x 00 = no address (addressing fields
* omitted). 0 x 01 = reserved. 0 x 02 = 16 bit short address.
* 0 x 03 = 64 bit extended address. */
uint8_t DstAddrMode;
/** The individual device address of the device for which the frame was
* intended. */
uint64_t DstAddr;
/** The communications status. */
uint8_t status;
} MLME_CommStatusInd_t;
Summary
MLME_CommStatusInd_t holds the MLME-COMM-STATUS.indication message structure
Description
None
Remarks
None