3.2.19 MLME_BeaconNotifyInd_t Struct
C
typedef struct mlme_beacon_notify_ind_tag {
/** This identifies the message as \ref MLME_BEACON_NOTIFY_INDICATION */
enum msg_code cmdcode;
/** The beacon sequence number. */
uint8_t BSN;
/** The PANDescriptor for the received beacon. */
WPAN_Pandescriptor_t PANDescriptor;
/** The beacon pending address specification. */
uint8_t PendAddrSpec;
/** The list of addresses of the devices for which the beacon source has
* data. */
uint8_t *AddrList;
/** The number of octets contained in the beacon payload of the beacon frame
* received by the MAC sublayer. */
uint8_t sduLength;
/** The set of octets comprising the beacon payload to be transferred from
* the MAC sublayerentity to the next higher layer. */
uint8_t *sdu;
} MLME_BeaconNotifyInd_t;
Summary
MLME_BeaconNotifyInd_t holds the MLME-BEACON-NOTIFY.indication message structure
Description
None
Remarks
None