2.24 2018 - September (ver 1.4)
START Configurator
Features
-
(#8947) Peripheral clocks can warn if frequency is outside limits
-
(#11504) If RTOS version of a driver is chosen, information is provided for usage and selection of RTOS if not present
-
(#11495) Added support for exporting MPLAB X projects for SAM devices
Bug Fixes
-
(#11381) Fix for caching the old release version in the Help page
-
(#11502) Fix for cleared out middlewares and drivers section from the tree view when the chosen driver/middleware count exceeds the available count
-
(#11492) Fix for updating wrong project properties when multiple projects are in AtmelStudio solution (Fix available from Studio extension acme 1.0.159.0 onwards)
- (#11409) Fix for resetting CCL or Event system resets other modules
-
(#11549) Removed confusing information if an older revision of specific devices are used in saved projects
-
(#11384) Added support for TCC2 for SAMDA1-SAMD21
START Content
New devices
- ATMega1609, ATmega1608, ATmega808
- ATTiny212, ATTiny412
- SAMC20E15A-AU/AZ/MU/MZ, SAMC20E16A-AU/AZ/MU/MZ, SAMC20E17A-AU/AZ/MU/MZ, SAMC20E18A-AU/AZ/MU/MZ
- SAMC20G15A-AU/AZ/MU/MZ, SAMC20G16A-AU/AZ/MU/MZ, SAMC20G17A-AU/AZ/MU/MZ, SAMC20G18A-AU/AZ/MU/MZ
- SAMC20J15A-AU/AZ/MU/MZ, SAMC20J16A-AU/AZ/MU/MZ, SAMC20J17A-AU/AZ/MU/MZ, SAMC20J18A-AU/AZ/MU/MZ
- SAMC21E15A-AU/AZ/MU/MZ, SAMC21E16A-AU/AZ/MU/MZ, SAMC21E17A-AU/AZ/MU/MZ, SAMC21E18A-AU/AZ/MU/MZ
- SAMC21G15A-AU/AZ/MU/MZ, SAMC21G16A-AU/AZ/MU/MZ, SAMC21G17A-AU/AZ/MU/MZ, SAMC21G18A-AU/AZ/MU/MZ
- SAMC21J15A-AU/AZ/MU/MZ, SAMC21J16A-AU/AZ/MU/MZ, SAMC21J17A-AU/AZ/MU/MZ, SAMC21J18A-AU/AZ/MU/MZ
- Renamed the device SAMC20J17A-UN to SAMC20J17A-UU
- Renamed the device SAMC20J18A-UN to SAMC20J18A-UU
- Renamed the device SAMC21J17A-UN to SAMC21J17A-UU
- Renamed the device SAMC21J18A-UN to SAMC21J18A-UU
- Refer migration guide to migrate the projects which uses older device names as mentioned above
New examples
- Added Low power weather station demo for SAML10-XPRO
- Added SmartEEPROM feature demonstration example for SAM D5x/E5x
Improvements
- Updated api documentation for spi_m_dma_set_baudrate api
Bug fixes
- Fixed SAME54 DFLL initialization issue for switching GCLK0 source
- Fixed project generation failure issue with PWM driver with TCC2 timer module
- Fixed IO port configuration order
- Fixed I2C slave driver for SAME54
- Fixed SPI DMA driver in HPL layer
- Changed SVC_handler to SVCall_handler for SAMD21/C2x/D5x/E5x devices
- USART max Baud-rate range is changed to 6.25MHz for SAMD5x/E5x devices
QTouch Configurator Updates 6.0
New Features
- Lump and low-power UI design addition
- Rubber band selection for creating Lump and Low-power sensors
- Added Low-power tab under parameters in QTouch Dashboard to configure low-power parameters
QTouch Library Updates 6.0
New Features
- Low-power feature support added with Event Driven and Software Driven approach. In Event Driven approach, either a button or lump sensor can be configured as low-power sensor. In software driven, multiple sensors button/slider/wheel/lump can be configured as low-power
- Low-power and Lump features are supported for following devices,
- ATTINY814, ATTINY816, ATTINY817,
- ATTINY1614, ATTINY1616, ATTINY1617,
- ATTINY3214, ATTINY3216, ATTINY3217,
- ATSAML10, ATSAML11
- A maximum of 16 lump can be created - if the device has sufficient memory. If Lump is configured as low-power with event-driven approach, the low-power detect threshold should be same as that of lump sensor
New examples
- QTouch Tiny3217 Xplained Pro Selfcap without Event System Example with OnBoard Sensors.
- QTouch Tiny3217 Xplained Pro Selfcap with Event System Example with OnBoard Sensors
- QTouch SAML10 Xplained Pro Selfcap Example with OnBoard Sensors
- QTouch SAML11 Xplained Pro TrustZone Lowpower Example
- SAME54 and SAMD51: Default clock configuration in START is changed from 24MHz to 48MHz as per recommended in datasheet
- SAMD1x: Acquisition module (library) is updated to ensure that bursting happens correctly on the configured Y lines
- Surface debug data is sent during burst again to ensure that seamless data is visible in surface GUI
- ATTiny81x/ATtiny161x/ATtiny321x: Acquisition module is updated to take care of a bug related to low-power sensor detect threshold (window-comparator threshold)
Device Support
-
The link below provides the list of devices supported in the QTouch Configurator 6.0 Release