2.26 2018 - June 25th (ver 1.3)
START Configurator
Features
- (#10902) Added ARM TrustZone support for Atmel Studio projects
- (#11341) Added support for exporting MPLAB X projects
- (#11228) Added descriptive dialog and notes on obsolete devices
- (#2750) Added information on how to add RTOS if RTOS version of drivers are selected
- (#11338) Activated color in Pinmux view when pin is configured
- (#10982) Changed default clock from 8 mhz to 16 mhz for Mega324BP Explain Pro board
- QTouch device support is added for SAML10 and SAML11 device family
- QTouch support is extended for the following device variants
- ATSAMD20E16B, ATSAMD20E15B, ATSAMD20E14B
- ATSAMD20G16B, ATSAMD20G15B, ATSAMD20G14B
- ATSAMD20J16B, ATSAMD20J15B, ATSAMD20J14B
- SAMHA1E14AB, SAMHA1E15AB, SAMHA1E16AB
Improvements
- QTouch Configurator Sub-tabs for Pins and Parameters tabs.
- Sync parameter values in the channel with enable and disable option.
- Sensor creation count status message.
- Notifications for SamL1x GCC support, L11 Trust Zone and AKS setting.
- Timeout issue fix for table tooltips in parameters tab.
- Tooltips for slider/wheel configuration table.
- Scroller parameters table field type change, sensor resolution and sensor deadband to enums.
- Surface utility and DV direct download links.
Bug Fixes
- Ensured frequencies are recalculated when changing clock options
Know issues
- Pre-configured clock system support does not work for SAME5x, D51 family touch projects
- IAR compiler for SAM L10 and SAM L11 family is not supported
UI Changes


-
If an RTOS version of a driver is selected, a button to access more information is added. From this, RTOS can be added to the project.

START Content
New devices
- ATSAML10D14A, ATSAML10D15A, ATSAML10D16A
- ATSAML10E14A, ATSAML10E15A, ATSAML10E16A
- ATSAML11D14A, ATSAML11D15A, ATSAML11D16A
- ATSAML11E14A, ATSAML11E15A, ATSAML11E16A
New middleware
- Added LwIP-v2.0.3 stack
- Added TrustZone Manager
New boards
- SAML10-XPRO
- SAML11-XPRO
New examples
- Added example to demonstrate OPAMP as a ADC gain Amplifier for SAML10-XPRO
- Added three example to demonstrate CPU performance with and without DMA along with ADC and USART for SAML10-XPRO
- Added TCC example to generate complementary waveform using TCC advance features for SAME54-XPRO
- Added example which uses the DMA Sequencing Operation supported by the ADC on SAM E54
- SAML11 Xplained Pro Self capacitance Shield Water Tolerant Secure Touch Example with QT7 extension
- SAML11 Xplained Pro Mutual capacitance Secure Touch Example with QT3 keypad extension
- SAML11 secure project with Trustzone middleware that should be used in association with non-secure touch example project
- SAML10 Xplained Pro Mutual capacitance Touch Example with QT3 keypad extension
- SAML10 Xplained Pro Self capacitance Shield Water Tolerant Touch Example with QT7 extension
Improvements
- Application code update for frequency hop module done for enhanced frequency hopping support.
- SCROLLER resolution and deadband parameters are modified to have enum values.
- CC values formula is corrected for the devices with four phase selfcap technology – SAML1x, SAME5x and SAMD51.
- Pre-scaler description for the nodes is corrected.
- Adjust QSPI parameter, increase speed and add bulk read/write test for XIP demo
Bug fixes
- Remove reserved ADC Negative Mux Input "I/O ground" option for SAML21/L22/R30/D51/E51/E53/E54
- Fix QSPI Flash erasing sequence
Know issues
- TrustZone support for "µVision from Keil" and "IAR Embedded Workbench" is not available for START projects now and it will be added soon