6.2.59 csinl Function
Calculates the complex sine function of a long double precision complex value.
Include
<complex.h>
Prototype
long double complex csinl(long double complex z);
Argument
-
z - value for which to return the complex sine
Return Value
Returns the complex sine of z.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <stdio.h>
#include <complex.h>
int main(void)
{
long double complex x, y;
x = -2.0 + 1.0*I;
y = csinl(x);
printf("The complex sine of %Lf + %Lfi is %Lf + %Lfi\n", creall(x), cimagl(x), creall(y), cimagl(y));
}
Example Output
The complex sine of -2.000000 + 1.000000i is -1.403119 + -0.489056i