6.2.15 carg Function
Calculates the argument of a double precision complex value.
Attention: This function is implemented only by MPLAB XC32 C
compilers.
Include
<complex.h>
Prototype
double complex carg(double complex z);
Argument
z- value for which to return the argument
Return Value
Returns the argument (or phase angle) of z in the interval
and with a branch cut along the negative real axis.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <stdio.h>
#include <complex.h>
int main(void)
{
double complex x, y;
x = -2.0 + 1.0*I;
y = carg(x);
printf("The complex argument of %f + %fi is %f + %fi\n", creal(x), cimag(x), creal(y), cimag(y));
}
Example Output
The complex argument of -2.000000 + 1.000000i is 2.677945 + 0.000000i