6.2.65 csqrtl Function
Calculates the complex square root of a long double precision complex value.
Include
<complex.h>
Prototype
long double complex csqrtl(long double complex z);
Argument
-
z - value for which to return the complex square root
Return Value
Returns the complex square root of z, in the right half plane, including the
imaginary axis, and with a branch cut along the negative real axis.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <stdio.h>
#include <complex.h>
int main(void)
{
long double complex x, y;
x = -2.0 + 1.0*I;
y = csqrtl(x);
printf("The complex square root of %Lf + %Lfi is %Lf + %Lfi\n", creall(x), cimagl(x), creall(y), cimagl(y));
}
Example Output
The complex square root of -2.000000 + 1.000000i is 0.343561 + 1.455347i