6.2.53 cprojl Function
Calculates the a projection of a long double precision complex value onto the Riemann sphere.
Include
<complex.h>
Prototype
long double complex cprojl(long double complex z);
Argument
-
z - value for which to calculate the projection
Return Value
Returns the a projection of a long double precision complex value, z, onto
the Riemann sphere. The projection is such that z is returned, except if
z is any complex infinity, in which case a positive infinity is
returned.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <stdio.h>
#include <complex.h>
#include <math.h>
int main(void)
{
long double complex x;
x = -INFINITY + 1.0*I;
y = cprojl(x);
printf("The Riemann plane projection of %Lf + %Lfi is %Lf + %Lfi\n", creall(x), cimagl(x), creall(y), cimagl(y));
}
Example Output
The Riemann plane projection of -inf + 1.000000i is inf + 0.000000i