6.2.47 conjl Function
Calculates the complex conjugate of a long double precision complex value.
Include
<complex.h>
Prototype
long double complex conjl(long double complex z);
Argument
-
z - value for which to return the complex conjugate
Return Value
Returns the complex conjugate of z, being the value of the argument with the
sign of the imaginary part reversed.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <stdio.h>
#include <complex.h>
int main(void)
{
long double complex x, y;
x = -2.0 + 1.0*I;
y = conjl(x);
printf("The complex conjugate of %Lf + %Lfi is %Lf + %Lfi\n", creall(x), cimagl(x), creall(y), cimagl(y));
}
Example Output
The complex conjugate of -2.000000 + 1.000000i is -2.000000 + -1.000000i