6.2.68 ctanl Function
Calculates the complex tangent function of a long double precision complex value.
Include
<complex.h>
Prototype
long double complex ctanl(long double complex z);
Argument
-
z - value for which to return the complex tangent
Return Value
Returns the complex tangent of z.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <stdio.h>
#include <complex.h>
int main(void)
{
long double complex x, y;
x = -2.0 + 1.0*I;
y = ctanl(x);
printf("The complex tangent of %Lf + %Lfi is %Lf + %Lfi\n", creall(x), cimagl(x), creall(y), cimagl(y));
}
Example Output
The complex tangent of -2.000000 + 1.000000i is 0.243458 + 1.166736i