6.2.40 cimagf Function
Calculates the imaginary part of a single precision complex value.
Attention: This function is implemented only by MPLAB XC32 C
compilers.
Include
<complex.h>
Prototype
float complex cimagf(float complex z);
Argument
z- value for which to return the imaginary part
Return Value
Returns the imaginary part of the single precision complex value z.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <stdio.h>
#include <complex.h>
int main(void)
{
float complex x;
x = -2.0 + 1.0*I;
printf("The imaginary part of %f + %fi is %f\n", crealf(x), cimagf(x), cimagf(x));
}
Example Output
The imaginary part of -2.000000 + 1.000000i is 1.000000