6.2.56 creall Function
Calculates the real part of a long double precision complex value.
Include
<complex.h>
Prototype
long double complex creall(long double complex z);
Argument
-
z - value for which to return the real part
Return Value
Returns the real part of the long double precision complex value z.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <stdio.h>
#include <complex.h>
int main(void)
{
long double complex x;
x = -2.0 + 1.0*I;
printf("The real part of %Lf + %Lfi is %Lf\n", creall(x), cimagl(x), creall(x));
}
Example Output
The real part of -2.000000 + 1.000000i is -2.000000