6.2.38 cexpl Function
Calculates the complex base- exponential of a long double precision complex value.
Include
<complex.h>
Prototype
long double complex cexpl(long double complex z);
Argument
-
z - value for which to return the complex base- exponential
Return Value
Returns the complex base- exponential of z.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <stdio.h>
#include <complex.h>
int main(void)
{
long double complex x, y;
x = -2.0 + 1.0*I;
y = cexpl(x);
printf("The complex base-e exponential of %Lf + %Lfi is %Lf + %Lfi\n", creall(x), cimagl(x), creall(y), cimagl(y));
}
Example Output
The complex base-e exponential of -2.000000 + 1.000000i is 0.073122 + 0.113881i