6.2.50 cpowl Function
Calculates the complex power function xy for long double
precision complex values.
Include
<complex.h>
Prototype
long double complex cpowl(long double complex x, long double complex
y);
Arguments
-
x - the base value
-
y - the exponent, or power, value
Return Value
Returns the complex power function xy, with a branch cut for the
base value (x) along the negative real axis.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <stdio.h>
#include <complex.h>
int main(void)
{
long double complex x, y, z;
x = -2.0 + 1.0*I;
y = 0.2 - 1.3*I;
z = cpowl(x, y);
printf("The complex value %Lf + %Lfi raised to the value %Lf + %Lfi is %Lf + %Lfi\n", creall(x), cimagl(x), creall(y), cimagl(y), creall(z), cimagl(z));
}
Example Output
The complex value -2.000000 + 1.000000i raised to the value 0.200000 + -1.300000i is 33.309896 + -18.656049i