6.2.46 conjf Function
Calculates the complex conjugate of a single precision complex value.
Attention: This function is implemented only by MPLAB XC32 C
compilers.
Include
<complex.h>
Prototype
float complex conjf(float complex z);
Argument
z- value for which to return the complex conjugate
Return Value
Returns the complex conjugate of z, being the value of the argument with
the sign of the imaginary part reversed.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <stdio.h>
#include <complex.h>
int main(void)
{
float complex x, y;
x = -2.0 + 1.0*I;
y = conjf(x);
printf("The complex conjugate of %f + %fi is %f + %fi\n", crealf(x), cimagf(x), crealf(y), cimagf(y));
}
Example Output
The complex conjugate of -2.000000 + 1.000000i is -2.000000 + -1.000000i