6.2.39 cimag Function
Calculates the imaginary part of a double precision complex value.
Attention: This function is implemented only by MPLAB XC32 C
compilers.
Include
<complex.h>
Prototype
double complex cimag(double complex z);
Argument
z- value for which to return the imaginary part
Return Value
Returns the imaginary part of the double precision complex value z.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <stdio.h>
#include <complex.h>
int main(void)
{
double complex x;
x = -2.0 + 1.0*I;
printf("The imaginary part of %f + %fi is %f\n", creal(x), cimag(x), cimag(x));
}
Example Output
The imaginary part of -2.000000 + 1.000000i is 1.000000