6.2.71 ctanhl Function
Calculates the complex hyperbolic tangent function of a long double precision complex value.
Include
<complex.h>
Prototype
long double complex ctanhl(long double complex z);
Argument
-
z - value for which to return the complex hyperbolic tangent
Return Value
Returns the complex hyperbolic tangent of z.
Example
See the notes at the beginning of this chapter or section for
information on using printf() or scanf()
(and other functions reading and writing the stdin or
stdout streams) in the example code.
#include <stdio.h>
#include <complex.h>
int main(void)
{
long double complex x, y;
x = -2.0 + 1.0*I;
y = ctanhl(x);
printf("The complex hyperbolic tangent of %Lf + %Lfi is %Lf + %Lfi\n", creall(x), cimagl(x), creall(y), cimagl(y));
}
Example Output
The complex hyperbolic tangent of -2.000000 + 1.000000i is -1.014794 + 0.033813i