10.8 EMAC Register Bit Definitions
The following tables define the bit definitions of the registers present in EMAC.
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:1] | Reserved | 0x0 | Reserved |
| 0 | Transmit control | 0x0 | TxEnable: Set this bit to enable DMA transmit
packet transfers. The bit is cleared by the built-in DMA controller whenever it encounters a Tx Underrun or Bus Error state. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:2] | Top 30 bits of Descriptor Address | 0x0. | When TxEnable is set by the host, the built-in DMA controller reads this register to discover the location in the host memory of the first transmit packet descriptor. |
| [1:0] | Ignored by the DMA controller | 0x0 | All descriptors are 32-bit aligned in the host memory. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:24] | Reserved | 0x0 | Reserved |
| [23:16] | TxPktCount | 0x0 | The 8-bit transmit packet counter that is incremented whenever the built-in DMA controller successfully transfers a packet, and is decremented whenever the host writes a '1' to bit '0' in this register. |
| [16:4] | Reserved | 0x0 | Reserved |
| 3 | BusError | 0x0 | When set, this indicates that a host slave split, retry or error response is received by the DMA controller. |
| 2 | Reserved | 0x0 | Reserved |
| 1 | TxUnderrun | 0x0 | Set whenever the DMA controller reads a '1' for the empty flag in the descriptor. |
| 0 | TxPktSent | 0x0 | When set, this indicates that one or more packets have been successfully transferred. Writing a '1' to this bit reduces the TxPktCount value by one. The bit is cleared whenever TxPktCount is zero. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:1] | Reserved | 0x0 | Reserved |
| 0 | Rx Enable | 0x0 | Setting this bit enables DMA receive packet transfers. The bit is cleared by the built-in DMA controller whenever it encounters an Rx overflow or bus error state. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:1] | Top 30 bits of Descriptor Address | 0x0 | When RxEnable is set by the host, the built-in DMA controller reads this register to discover the location in the host memory of the first receive packet descriptor. |
| 0 | Ignored by the DMA controller | 0x0 | All descriptors are 32-bit aligned in the host memory. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:24] | Reserved | 0x0 | Reserved |
| [23:16] | RxPktCount | 0x0 | The 8-bit receive packet counter that is incremented whenever the built-in DMA controller successfully transfers a packet, and is decremented whenever the host writes a “1” to bit zero of this register. |
| [16:4] | Reserved | 0x0 | Reserved |
| 3 | BusError | 0x0 | When set, this indicates that a host slave split, retry or error response is received by the DMA controller. |
| 2 | RxOverflow | 0x0 | Set whenever the DMA controller reads a zero empty flag in the descriptor it is processing. |
| 1 | Reserved | 0x0 | Reserved |
| 0 | RxPktReceived | 0x0 | When set, this indicates that one or more packets have been successfully transferred. Writing a “1” to this bit reduces the RxPktCount value by one. The bit is cleared whenever RxPktCount is zero. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:8] | Reserved | 0x0 | Reserved |
| 7 | Bus Error Mask | 0x0 | Setting this bit to “1” enables the Bus Error bit in the DMARxStatus register as an interrupt source. |
| 6 | Rx Overflow Mask | 0x0 | Setting this bit to “1” enables the RxOverflow bit in the DMARxStatus register as an interrupt source. |
| 5 | Reserved | 0x0 | Reserved |
| 4 | RxPktReceived Mask | 0x0 | Setting this bit to “1” enables the RxPktReceived bit in the DMARxStatus register as an interrupt source. |
| 3 | Bus Error Mask | 0x0 | Setting this bit to “1” enables the Bus Error bit in the DMATxStatus register as an interrupt source. |
| 2 | Reserved | 0x0 | Reserved |
| 1 | Tx Underrun Mask | 0x0 | Setting this bit to “1” enables the TxUnderrun bit in the DMATxStatus register as an interrupt source. |
| 0 | TxPktSent Mask | 0x0 | Setting this bit to “1” enables the TxPktSent bit in the DMATxStatus register as an interrupt source. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:8] | Reserved | 0x0 | Reserved |
| 7 | Bus Error | 0x0 | This is set to “1” to record a receive bus error interrupt when the Bus Error bit in the DMARxStatus register and bit 7 of the DMAIntrMask register are both set. |
| 6 | Rx Overflow | 0x0 | This is set to “1” to record an Rx overflow interrupt when the RxOverflow bit in the DMARxStatus register and bit 6 of the DMAIntrMask register are both set. |
| 5 | Reserved | 0x0 | Reserved |
| 4 | RxPktReceived | 0x0 | This is set to “1” to record a RxPktReceived interrupt when the RxPktReceived bit in the DMARxStatus register and bit 4 of the DMAIntrMask register are both set. |
| 3 | Bus Error | 0x0 | This is set to “1” to record a transmit bus error interrupt when the Bus Error bit in the DMATxStatus register and bit 3 of the DMAIntrMask register are both set. |
| 2 | Reserved | 0x0 | Reserved |
| 1 | Tx Underrun | 0x0 | This is set to “1” to record a Tx underrun interrupt when the TxUnderrun bit in the DMATxStatus register and bit 1 of the DMAIntrMask register are both set. |
| 0 | TxPktSent | 0x0 | This is set to “1” to record a TxPktSent interrupt when the TxPktSent bit in the DMATxStatus register and bit 0 of the DMAIntrMask register are both set. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| 31 | SOFT RESET | 0x1 | Setting this bit will put all modules within the PE-MCXMAC in the reset except the Host Interface. |
| 30 | SIMULATION RESET | 0x0 | Setting this bit will reset those registers, such as the random backoff timer, which are not controlled by the normal resets (simulation only). |
| [29:20] | Reserved | 0x0 | Reserved |
| 19 | RESET RX MAC CONTROL | 0x0 | Setting this bit puts the PERMC Receive MAC control in reset. |
| 18 | RESET TX MAC CONTROL | 0x0 | Setting this bit puts the PETMC Transmit MAC control in reset. |
| 17 | RESET RX FUNCTION | 0x0 | Setting this bit puts the PERFN receive function block in reset. PERFN block performs the receive frame protocol. |
| 16 | RESET TX FUNCTION | 0x0 | Setting this bit puts the PETFN transmit function block in reset. PETFN block performs the frame transmission protocol. |
| [15:9] | Reserved | 0x0 | Reserved |
| 8 | LOOP BACK | 0x0 | Setting this bit causes the PETFN MAC transmit outputs to be looped back to the MAC receive inputs. Clearing this bit results in normal operation. |
| [7:6] | Reserved | 0x0 | Reserved |
| 5 | RECEIVE FLOW CONTROL ENABLE | 0x0 | Setting this bit causes the PERFN receive. MAC control to detect and act on PAUSE flow control frames. Clearing this bit causes the receive MAC control to ignore PAUSE flow control frames. |
| 4 | TRANSMIT FLOW CONTROL ENABLE | 0x0 | Setting this bit allows the PETMC transmit. MAC control sends PAUSE flow control frames when requested by the system. Clearing this bit prevents the transmit MAC control from sending flow control frames. |
| 3 | SYNCHRONIZED RECEIVE ENABLE | 0x0 | This field is read only and indicates that the receive enable is synchronized to the receive stream. |
| 2 | RECEIVE ENABLE | 0x0 | Setting this bit allows the MAC to receive frames from the PHY. Clearing this bit prevents the reception of the frames. |
| 1 | SYNCHRONIZED TRANSMIT ENABLE | 0x0 | This field is read only and indicates that the transmit enable is synchronized to the transmit stream. |
| 0 | TRANSMIT ENABLE | 0x0 | Setting this bit allows the MAC to transmit frames from the system. Clearing this bit prevents the transmission of the frames. |
| Bit Number | Name | Reset Value | Description | ||
|---|---|---|---|---|---|
| [31:16] | Reserved | 0x0 | Reserved | ||
| [15:12] | PREAMBLE LENGTH | 0x7 | This field determines the length of the preamble field of the packet in bytes. Default is ‘0x7’. | ||
| [9:8] | INTERFACE MODE | 0x0 | This field determines the type of interface the MAC is connected to. The Interface mode settings are as follows: | ||
| Interface mode | Bit 9 | Bit 8 | |||
| Reserved | 0 | 0 | |||
| Nibble mode (10/100 Mbps MII/RMII/SMII, … ) | 0 | 1 | |||
| Byte mode (1000 Mbps GMII/TBI) | 1 | 0 | |||
| Reserved | 1 | 1 | |||
| [7:6] | Reserved | 0x0 | Reserved | ||
| 5 | HUGE FRAME ENABLE | 0x0 | Set this bit to transmit and receive the frames that are longer than the MAXIMUM FRAME LENGTH. Clear this bit to have the MAC limits the length of frames at the MAXIMUM FRAME LENGTH value. | ||
| 4 | LENGTH FIELD CHECKING | 0x0 | Set this bit to cause the MAC to check the frame’s length field to ensure it matches the actual data field length. Clear this bit if no length field checking is desired. | ||
| 3 | Reserved | 0x0 | Reserved | ||
| 2 | PAD/CRC ENABLE | 0x0 | Set this bit to have the MAC pads all the short frames and appends a CRC to every frame whether or not padding is required. Clear this bit if frames, presented to the MAC, have a valid length and contain a CRC. | ||
| 1 | CRC ENABLE | 0x0 | Set this bit to have the MAC appends a CRC to all the frames. Clear this bit if frames that are presented to the MAC, have a valid length and contain a valid CRC. If the PAD/CRC ENABLE configuration bit or the per-packet PAD/CRC ENABLE is set, CRC ENABLE is ignored. | ||
| 0 | FULL-DUPLEX | 0x0 | Setting this bit configures the PE-MCXMAC to operate in full-duplex mode. Clearing this bit configures the PE-MCXMAC to operate in half-duplex mode only. | ||
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| 31 | Reserved | 0x0 | Reserved |
| [30:24] | NON-BACK-TO-BACK INTER-PACKET-GAP PART 1 (IPGR1) | 0x40 | This programmable field represents the optional carrier Sense window, which is referenced in the IEEE 802.3/4.2.3.2.1 ‘Carrier Deference’. If a carrier is detected during the timing of IPGR1, the MAC defers to the carrier. However, the carrier becomes active after IPGR1; the MAC continues timing IPGR2 and transmit, knowingly causing a collision. This ensures fair access to the medium. The permitted range of values is 0x0 to IPGR2. Default is 0x40. |
| 23 | Reserved | 0x0 | Reserved |
| [22:16] | NON-BACK-TO-BACK INTER-PACKET-GAP PART 2 (IPGR2) | 0x60 | This programmable field represents the Non-Back-to-Back Inter-Packet-Gap in the bit times, which represent the minimum inter packet gap (IPG) of 96 bits. |
| [15:8] | MINIMUM IFG ENFORCEMENT | 0x50 | This programmable field represents the minimum size of management gap (IFG) to enforce between frames (expressed in bit times). A frame whose IFG is less than the programmed minimum IFG enforcement value is dropped. The default setting of 0x50 represents half of the nominal minimum IFG which is 160 bits. |
| 7 | Reserved | 0x0 | Reserved |
| [6:0] | BACK-TO-BACK INTER-PACKET-GAP | 0x60 | This programmable field represents the IPG between Back-to-Back packets (expressed in bit times). This is the IPG parameter used exclusively in full-duplex mode when two transmit packets are sent back-to-back. Set this field to the desired number of bits. The default setting of 0x60 represents the minimum IPG of 96 bits. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:24] | Reserved | 0x0 | Reserved |
| [23:20] | ALTERNATE BINARY EXPONENTIAL BACKOFF TRUNCATION | 0xA | This field is used when ALTERNATE BINARY EXPONENTIAL BACKOFF ENABLE is set. The value programmed is substituted for the Ethernet standard value of ten. Default is ‘0xA’. |
| 19 | ALTERNATE BINARY EXPONENTIAL BACKOFF ENABLE | 0x0 | Setting this bit configures the Tx MAC to use the ALTERNATE BINARY EXPONENTIAL BACKOFF TRUNCATION setting instead of the 802.3 standard tenth collision. Clearing this bit causes the Tx MAC to follow the standard binary exponential backoff rule. |
| 18 | BACKPRESSURE NO BACKOFF | 0x0 | Setting this bit configures the Tx MAC to immediately re-transmit following a collision during back pressure operation. Clearing this bit causes the Tx MAC to follow the binary exponential backoff rule. |
| 17 | NO BACKOFF | 0x0 | Setting this bit configures the Tx MAC to immediately re-transmit following a collision. Clearing this bit causes the Tx MAC to follow the binary exponential backoff rule. |
| 16 | EXCESSIVE DEFER | 0x1 | Setting this bit configures the Tx MAC to allow the transmission of a packet that has been excessively deferred. Clearing this bit causes the Tx MAC to abort the transmission of a packet that has been excessively deferred. |
| [15:12] | RETRANSMISSION MAXIMUM | 0xF | This is a programmable field specifying the number of retransmission attempts following a collision before aborting the packet due to excessive collisions. The standard specifies the maximum number of attempts to be 0xF (15d). |
| [11:10] | Reserved | 0x0 | Reserved |
| [9:0] | COLLISION WINDOW | 0x37 | This programmable field represents the slot time or collision window during which collisions might occur in a properly configured network. Since the collision window starts at the beginning of the transmission, the preamble and start frame delimiter (SFD) are included. The default of 0x37 (55d) corresponds to the count of the frame bytes at the end of the window. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:16] | Reserved | 0x0 | Reserved |
| [15:0] | MAXIMUM FRAME LENGTH | 0x600 | This programmable field sets the maximum frame size in both the transmit and receive directions. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:4] | Reserved | 0x0 | Reserved |
| 3 | MAXIMUM FRAME LENGTH | 0x0 | Setting this bit causes the MAC to backoff for the maximum possible length of time. This test bit is used to predict the backoff times in half-duplex mode. |
| 2 | REGISTERED TRANSMIT FLOW ENABLE | 0x0 | Registered transmit half-duplex flow enable. |
| 1 | TEST PAUSE | 0x0 | Setting this bit allows the MAC to be paused via the host interface for the testing purposes. |
| 0 | SHORTCUT SLOT TIME | 0x0 | This bit allows the slot time counter to expire regardless of the current count. This bit is for the testing purposes only. |
| Bit Number | Name | Reset Value | Description | |||
|---|---|---|---|---|---|---|
| 31 | RESET MII MGMT | 0x0 | Setting this bit resets MII Mgmt. Clearing this bit allows MII Mgmt to perform Mgmt read/write cycles as requested via the Host Interface. | |||
| 30:6 | Reserved | 0x0 | Reserved | |||
| 5 | SCAN AUTO INCREMENT | 0x0 | Setting this bit causes MII Mgmt to continually read from a set of PHYs of contiguous address space. The starting address of the PHY is specified by the content of the PHY address field, which is recorded in the MII Mgmt Address register. Up to 31 PHY contiguous address space can be addressed. The last PHY, which is to be queried in this read sequence, is the one residing at address 0x31, after which the read sequence returns to the PHY, specified by the PHY address field. | |||
| 4 | PREAMBLE SUPPRESSION | 0x0 | Setting this bit causes MII Mgmt to suppress preamble generation and reduce the Mgmt cycle from 64 clocks to 32 clocks. This is in accordance with the IEEE 802.3/22.2.4.4.2. Clearing this bit causes MII Mgmt to perform Mgmt read/write cycles with the 64 clocks of preamble. | |||
| 3 | Reserved | 0x0 | Reserved | |||
| 2:0 | MGMT CLOCK SELECT | 0x0 | This field determines the clock frequency of the management data clock (MDC). Following are the MGMT Clock Select Encoding programming fields: | |||
| Mgmt Clock Select | 2 | 1 | 0 | |||
| Source Clock divided by 4 | 0 | 0 | 0 | |||
| Source Clock divided by 4 | 0 | 0 | 1 | |||
| Source Clock divided by 6 | 0 | 1 | 0 | |||
| Source Clock divided by 8 | 0 | 1 | 1 | |||
| Source Clock divided by 10 | 1 | 0 | 0 | |||
| Source Clock divided by 14 | 1 | 0 | 1 | |||
| Source Clock divided by 20 | 1 | 1 | 0 | |||
| Source Clock divided by 28 | 1 | 1 | 1 | |||
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| 31:2 | Reserved | 0x0 | Reserved |
| 1 | SCAN CYCLE | 0x0 | This bit causes MII Mgmt to perform Read cycles continuously. This is useful to monitor Link Fail. |
| 0 | READ CYCLE | 0x0 | This bit causes MII Mgmt to perform a single Read cycle. The Read data is returned in Register 0xC (MII Mgmt Read Data). |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:13] | Reserved | 0x0 | Reserved |
| [12:8] | PHY ADDRESS | 0x00 | This field represents the 5-bit PHY address field used in Mgmt cycles. Up to 31 PHYs can be addressed (0 is reserved). |
| [4:0] | REGISTER ADDRESS | 0x00 | This field represents the 5-bit register address field of Mgmt cycles. Up to 32 registers can be accessed. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:16] | Reserved | 0x0 | Reserved |
| [15:0] | MII MGMT CONTROL | 0x0 | When written, an MII Mgmt write cycle is performed using the 16-bit data and the pre-configured PHY and register addresses from the MII Mgmt Register (0x0A). |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:16] | Reserved | 0x0 | Reserved |
| [15:0] | MII MGMT STATUS (PHY STATUS) | 0x0 | Following an MII Mgmt read cycle, the 16-bit data can be read from this location. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:3] | Reserved | 0x0 | Reserved |
| 2 | NOT VALID | 0x0 | When “1” is returned, this indicates MII Mgmt Read cycle is not completed and the Read Data is not yet validated. |
| 1 | SCANNING | 0x0 | When “1” is returned, this indicates a scan operation (continuous MII Mgmt Read cycles) is in progress. |
| 0 | BUSY | 0x0 | When “1” is returned, this indicates MII Mgmt block is currently performing an MII Mgmt read or write cycle. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| 31 | RESET INTERFACE MODULE | 0x0 | Setting this bit resets the interface module. Clearing this bit allows for the normal operation. This bit can be used in the place of bits 23, 15, and 7, when just 1 interface module is connected. |
| [30:28] | Reserved | 0x0 | Reserved |
| 27 | TBIMODE | 0x0 | Setting this bit configures the A-RGMII module to expect TBI signals at the GMII interface. This bit should not be asserted unless this mode is being used. |
| 26 | GHDMODE | 0x0 | Setting this bit configures the A-RGMII module to expect half-duplex GMII at the GMII interface. |
| 25 | LHDMODE | 0x0 | Setting this bit configures the A-RGMII module to expect 10 or 100 half-duplex MII at the GMII interface. This bit should not be asserted unless this mode is being used. |
| 24 | PHY MODE | 0x0 | Setting this bit configures the PESMII serial MII module to be in PHY mode. Link characteristics are taken directly from the Rx segments supplied by the PHY. Clearing this bit configures the PESMII to be in MAC to MAC mode. In this configuration, the Serial MII module reverts to the pre-defined settings of 100 Mbps, full-duplex. |
| 23 | RESET PERMII | 0x0 | Setting this bit resets the PERMII module. Clearing this bit allows for normal operation. |
| [22:17] | Reserved | 0x0 | Reserved |
| 16 | SPEED | 0x0 | This bit configures the PERMII Reduced MII module with the current operating speed. When set, 100 Mbps mode is selected. When cleared, 10 Mbps mode is selected. |
| 15 | RESET PE100X | 0x0 | This bit resets the 4B/5B symbol encipher/decipher logic. |
| [14:11] | Reserved | 0x0 | Reserved |
| 10 | FORCE QUIET | 0x0 | When enabled, the transmit data is cleared which allows the contents of the cipher to be the output. When cleared, the normal operation is enabled. This affects the 4B/5B symbol encipher/decipher logic module only. |
| 9 | NO CIPHER | 0x0 | When enabled, the raw transmit 5B symbols are transmitted without ciphering. When disabled, the normal ciphering occurs. This affects the 4B/5B symbol encipher/decipher logic module only. |
| 8 | DISABLE LINK FAIL | 0x0 | When enabled, the 330 ms Link Fail timer is disabled, allowing shorter simulations. Removes the 330 ms link-up time before reception of streams is allowed. When cleared, normal operation occurs. Affects 4B/5B symbol encipher/decipher logic module only. |
| 7 | Reserved | 0x0 | Reserved |
| [6:1] | Reserved | 0x0 | Reserved |
| 0 | ENABLE JABBER PROTECTION | 0x0 | This bit enables the jabber protection logic. Jabber is the condition where a transmitter is stuck on for longer than 50 ms to prevent other stations from transmitting. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:11] | Reserved | 0x0 | Reserved |
| 10 | Reserved | 0x0 | Reserved |
| 9 | EXCESS DEFER | 0x0 | This bit sets when the MAC excessively defers a transmission. It clears when read. This bit latches high. |
| 8 | CLASH | 0x0 | When read as a “1”, the Serial MII module is
in the MAC to MAC mode with the partner in 10 Mbps and/or half-duplex mode
indicative of a configuration error. When read as a “0”, the Serial MII module is either in PHY mode or in a properly configured MAC to MAC mode. |
| 7 | JABBER | 0x0 | When read as a “1”, the Serial MII PHY detects a jabber condition on the link. When read as a “0”, the Serial MII PHY does not detect a jabber condition. |
| 6 | LINK OK | 0x0 | When read as a “1”, the Serial MII PHY detects a valid link. When read as a “0”, the Serial MII PHY does not detect a valid link. |
| 5 | FULL DUPLEX | 0x0 | When read as a “1”, the Serial MII PHY operates in full-duplex mode. When read as a “0”, the Serial MII PHY operates in half-duplex mode. |
| 4 | SPEED | 0x0 | When read as a “1”, the Serial MII PHY operates at 100 Mbps mode. When read as a “0”, the Serial MII PHY operates at 10 Mbps. |
| 3 | LINK FAIL | 0x0 | When read as a “1”, the MII Management module reads the PHY link fail register to be 1’. When read as a “0”, the MII Management module reads the PHY link fail register to be 0’. Note: For asynchronous host accesses, this bit must be read at least once every scan read cycle of the PHY. |
| 2 | Reserved | 0x0 | Reserved |
| 1 | Reserved | 0x0 | Reserved |
| 0 | Reserved | 0x0 | Reserved |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:24] | STATION ADDRESS | 0x0 | This field holds the first octet of the station address. |
| [23:16] | STATION ADDRESS | 0x0 | This field holds the second octet of the station address. |
| [15:8] | STATION ADDRESS | 0x0 | This field holds the third octet of the station address. |
| [7:0] | STATION ADDRESS | 0x0 | This field holds the fourth octet of the station address. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:24] | STATION ADDRESS | 0x0 | This field holds the fifth octet of the station address. |
| [23:16] | STATION ADDRESS | 0x0 | This field holds the sixth octet of the station address. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:21] | Reserved | 0x0 | Reserved |
| 20 | ftfenrply | 0x0 | This is a read only bit. When asserted, the FIFO transmit interface is enabled. When de-asserted, the FIFO transmit interface is disabled. The bit should be polled until it reaches the expected value. |
| 19 | stfenrply | 0x0 | This is a read only bit. When asserted, the FIFO PE-MCXMAC transmit interface module is enabled. When de-asserted, the FIFO PE-MCXMAC transmit interface module is disabled. The bit should be polled until it reaches the expected value. |
| 18 | frfenrply | 0x0 | This is a read only bit. When asserted, the FIFO receive interface module is enabled. When de-asserted, the FIFO receive interface module is disabled. The bit should be polled until it reaches the expected value. |
| 17 | srfenrply | 0x0 | This is a read only bit. When asserted, the FIFO PE-MCXMAC receive interface module is enabled. When de-asserted, the FIFO PE-MCXMAC receive interface module is disabled. The bit should be polled until it reaches the expected value. |
| 16 | wtmenrply | 0x0 | When asserted, the FIFO PE-MCXMAC watermark module is enabled. When de-asserted, the FIFO PE-MCXMAC watermark module is disabled. The bit should be polled until it reaches the expected value. |
| [15:13] | Reserved | 0x0 | Reserved |
| 12 | ftfenreq | 0x0 | When asserted, this bit requests to enable
the FIFO fabric transmit interface module. When de-asserted, this bit requests to disable the FIFO Fabric transmit interface module. |
| 11 | stfenreq | 0x0 | When asserted, this bit requests to enable
the FIFO
PE-MCXMAC transmit interface module. When de-asserted, this bit requests to disable the FIFO PE-MCXMAC transmit interface module. |
| 10 | frfenreq | 0x0 | When asserted, this bit requests to enable
the FIFO fabric receive interface module. When de-asserted, this bit requests to disable of the FIFO fabric receive interface module. |
| 9 | srfenreq | 0x0 | When asserted, this bit requests to enable
the FIFO
PE-MCXMAC receive interface module. When de-asserted, this bit requests to disable the FIFO PE-MCXMAC receive interface module. |
| 8 | wtmenreq | 0x0 | When asserted, this bit requests to enable
the FIFO
PE-MCXMAC Watermark module. When de-asserted, this bit requests to disable the FIFO PE-MCXMAC watermark module. |
| [7:5] | Reserved | 0x0 | Reserved |
| 4 | hstrstft | 0x0 | When asserted, this bit places the FIFO Fabric transmit interface module in reset. |
| 3 | hstrstst | 0x0 | When asserted, this bit places the FIFO PE-MCXMAC transmit interface module in reset. |
| 2 | hstrstfr | 0x0 | When asserted, this bit places the FIFO Fabric receive interface module in reset. |
| 1 | hstrstsr | 0x0 | When asserted, this bit places the FIFO PE-MCXMAC receive interface module in reset. |
| 0 | hstrstwt | 0x0 | When asserted, this bit places the FIFO PE-MCXMAC watermark module in reset. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:28] | Reserved | 0x0 | Reserved |
| [27:16] | cfgsrth[11:0] | 0xFFF | This bit represents the minimum number of 4 byte locations, which are simultaneously stored in the receive RAM, relative to the beginning of the frame being input, before the fabric receive ready may be asserted. |
| [15:0] | cfgxoffrtx | 0xFFFF | This bit represents the number of pause quanta after an XOFF pause frame is acknowledged, until the A-MCXFIFO re-asserts pause request if the A-MCXFIFO receive storage level remains higher than the low watermark. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:29] | Reserved | 0x0 | Reserved |
| [28:16] | cfghwm | 0x1FFF | This bit represents the maximum number of 4 byte words that are simultaneously stored in the receive RAM before the transmit flow control enables and pause value facilitates an XOFF pause control frame. |
| [15:13] | Reserved | 0x0 | Reserved |
| [12:0] | cfglwm | 0x1FFF | This bit represents the minimum number of 4 byte words that are simultaneously stored in the receive RAM before transmit flow control enables and pause value facilitates an XON pause control frame in response to a previously transmitted XOFF pause control frame. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:28] | Reserved | 0x0 | Reserved |
| [27:16] | cfghwmft | 0xFFF | This hex value represents the maximum number of 4 byte locations, which are simultaneously stored in the transmit RAM before the fthwm is asserted. The fthwm is asserted whenever the amount of four byte locations, used in the transmit FIFO data RAM, exceeds the value programmed in the cfghwmft host register. |
| [15:12] | Reserved | 0x0 | Reserved |
| [11:0] | cfgftth | 0xFFF | This bit represents the minimum number of 4 byte locations which are simultaneously stored in the transmit RAM, relative to the beginning of the frame being input, before transmit packet start of frame is asserted. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:18] | Reserved | 0x0 | Reserved |
| [17:0] | hstfltrfrm | 0x0 | These configuration bits are used to signal
the drop frame conditions internal to the A-MCXFIFO. The bits correspond to the receive statistics vector input to A-MCXFIFO on a one per one basis. Receive statistics vector indicates the characteristics of the current receive frame and is input to A-MCXFIFO. The setting of this bits along with their don’t care values in the hstfltrfrmdc not asserted, create the filter that drops the receive frame if the receive frame does not pass through the acceptable conditions. For example, if it is needed to drop a frame that contains a receive error, least significant fourth bit is set, and all receive frames that have frame receive error in receive statistics vector asserted are dropped. The hstfltrfrm bit and their corresponding receive statistics vector is as follows: Bit Description 17: System receive unicast address 16: Truncated frame 15: Receive long event 14: VLAN Tagged frame: frame’s length/type field contained 0x8100 which is the VLAN protocol identifier 13: Frame was an unsupported Op-code 12: Frame was a PAUSE control frame 11: Long event detected 10: Frame contained a dribble nibble 9: Broadcast address detected 8: Multicast address detected 7: Reception OK 6: Length/Type field was neither a length nor type 5: Frame’s length field out of range 4: Frame contained a CRC error 3: Frame contained a code error 2: False carrier previously seen 1: RX_DV event previously seen 0: Whether or not a prior packet was dropped |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:23] | Reserved | 0x0 | Reserved |
| 22 | cfghdplx | 0x0 | Assertion of this bit configures the A-MCXFIFO to enable the half-duplex as a flow control mechanism. De-assertion of this bit configures the A-MCXFIFO to enable pause frames as a flow control mechanism. |
| 21 | srfull | 0x0 | Assertion of this read-only bit indicates that the maximum capacity of the receive FIFO storage is met or exceeded. |
| 20 | hstsrfullclr | 0x0 | This bit should be written when it is desired to clear the srfull indicator bit. After the hstfullclr assertion, the srfull should be read until it becomes unasserted. |
| 19 | cfgbytmode | 0x0 | This bit should be asserted when the PE-MCXMAC is configured for GMII mode. |
| 18 | hstdrplt64 | 0x0 | Setting this bit causes the frame to be dropped if a receive frame is less than 64 bytes in length. |
| [17:0] | hstfltrfrmdc | 0X3FFFF | These configuration bits indicate which
receive statistics vectors are don’t care for A-MCXFIFO frame drop circuitry.
Receive statistics vector indicates the characteristics of the current receive
frame. Setting of the hstfltrfrmdc bit, indicates a don’t care for the receive statistics vector bit. These bits corresponds to receive statistics vector on a one per one basis. The hstfltrfrmdc bit and their corresponding receive statistics vector is as follows: Bit Description 17: System receive unicast address 16: Truncated frame 15: Receive long event 14: VLAN Tagged frame: frame’s length/type field contained 0x8100 which is the VLAN protocol identifier 13: Frame was an unsupported Op-code 12: Frame was a PAUSE control frame 11: Long event detected 10: Frame contained a dribble nibble 9: Broadcast address detected 8: Multicast address detected 7: Reception OK 6: Length/Type field was neither a length nor type 5: Frame’s length field is out of range 4: Frame contained a CRC error 3: Frame contained a code error 2: False carrier previously seen 1: RX_DV event previously seen 0: Whether or not a prior packet was dropped |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| 31 | hsttramwreq | 0x0 | Host transmit RAM write request |
| 30 | hsttramwack | 0x0 | Host transmit RAM write acknowledge |
| [29:24] | Reserved | 0x0 | Reserved |
| [23:16] | hsttramwdat [39:32] | 0x0 | Host transmit RAM write data This is the upper byte of the transmit FIFO RAM data that is written at the address of hsttramwadx[10:0], if hsttramwadx[12] is negated and hsttramwreq is asserted. |
| [15:13] | Reserved | 0x0 | Reserved |
| [12:0] | hsttramwadx | 0x0 | Host transmit RAM write address |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:0] | hsttramwdat | 0x0 | Host transmit RAM write data |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| 31 | hsttramrreq | 0x0 | Host transmit RAM read request |
| 30 | hsttramrack | 0x0 | Host transmit RAM read acknowledge |
| [29:24] | Reserved | 0x0 | Reserved |
| [23:16] | hsttramrdat | 0x0 | Host transmit RAM read data. This is the upper byte of the transmit FIFO RAM data that was read at the address of the hsttramwadx[10:0], if the hsttramwadx[12] is negated and the hsttramwreq is asserted. |
| [15:13] | Reserved | 0x0 | Reserved |
| [12:0] | hsttramradx | 0x0 | Host transmit RAM read address |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:0] | hsttramrdat | 0x0 | Host transmit RAM read data |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| 31 | hstrramwreq | 0x0 | Host receive RAM write request |
| 30 | hstrramwack | 0x0 | Host receive RAM write acknowledge |
| [29:24] | Reserved | 0x0 | Reserved |
| [23:16] | hstrramwdat[39:32] | 0x0 | Host receive RAM write data This is the upper byte of the receive FIFO RAM data that is written at the address of the hstrramwadx[11:0], if the hstrramwadx[13] is negated and the hstrramwreq is asserted. |
| [15:14] | Reserved | 0x0 | Reserved |
| [13:0] | hsttramwadx | 0x0 | Host receive RAM write address |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:0] | hstrramwdat | 0x0 | Host receive RAM write data |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| 31 | hstrramrreq | 0x0 | Host receive RAM read request |
| 30 | hstrramrack | 0x0 | Host receive RAM read acknowledge |
| [29:24] | Reserved | 0x0 | Reserved |
| [23:16] | hstrramrdat [39:32] | 0x0 | Host receive RAM read data This is the upper byte of the receive FIFO RAM data that is read at the address of the hstrramwadx[10:0] if the hstrramwadx[13] is negated and the hstrramwreq is asserted. |
| [15:14] | Reserved | 0x0 | Reserved |
| [13:0] | hstrramradx [13:0] | 0x0 | Host receive RAM read address |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:0] | hstrramrdat | 0x0 | Host receive RAM read data |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:18] | Reserved | 0x0 | Reserved |
| [17:0] | TR64 | 0x0 | Transmit and receive 64 byte frame counter: Incremented for each good or bad transmitted and received frame, which is 64 bytes in length inclusive (excluding framing bits but including FCS bytes). |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:18] | Reserved | 0x0 | Reserved |
| [17:0] | TR127 | 0x0 | Transmit and receive 65 to 127 byte frame counter: Incremented for each good or bad, transmitted and received frame, which is 65 to 127 bytes in length inclusive (excluding framing bits but including FCS bytes). |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:18] | Reserved | 0x0 | Reserved |
| [17:0] | TR255 | 0x0 | Transmit and receive 128 to 255 byte frame counter: Incremented for each good or bad, transmitted and received frame, which is 128 to 255 bytes in length inclusive (excluding framing bits but including FCS bytes). |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:18] | Reserved | 0x0 | Reserved |
| [17:0] | TR511 | 0x0 | Transmit and receive 256 to 511 byte frame counter: Incremented for each good or bad, transmitted and received frame, which is 256 to 511 bytes in length inclusive (excluding framing bits but including FCS bytes). |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:18] | Reserved | 0x0 | Reserved |
| [17:0] | TR1K | 0x0 | Transmit and receive 512 to 1023 byte frame counter: Incremented for each good or bad, transmitted and received frame, which is 512 to 1023 bytes in length inclusive (excluding framing bits but including FCS bytes). |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:18] | Reserved | 0x0 | Reserved |
| [17:0] | TRMAX | 0x0 | Transmit and receive 1024 to 1518 byte frame counter: Incremented for each good or bad, transmitted and received frame, which is 1024 to 1518 bytes in length inclusive (excluding framing bits but including FCS bytes). |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:18] | Reserved | 0x0 | Reserved |
| [17:0] | TRMGV | 0x0 | Transmit and receive 1519 to 1522 byte VLAN frame counter: Incremented for each good Virtual Local Area Network (VLAN) transmitted and received frame which is 1519 to 1522 bytes in length inclusive (excluding framing bits but including FCS bytes). |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:24] | Reserved | 0x0 | Reserved |
| [23:0] | RBYT | 0x0 | Receive byte frame counter: The statistic counter register is incremented by the byte count of all the frames received, including those in the bad packets, excluding framing bits but including FCS bytes. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:18] | Reserved | 0x0 | Reserved |
| [17:0] | RPKT | 0x0 | Receive packet counter: Incremented for each frame received packet (including bad packets, all the unicast, broadcast, and multicast packets). |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:12] | Reserved | 0x0 | Reserved |
| [11:0] | RFCS | 0x0 | Receive FCS error counter: Incremented for each frame received that has an integral 64 to 1518 length and contains a FCS error. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:18] | Reserved | 0x0 | Reserved |
| [17:0] | RMAC | 0x0 | Receive multicast packet counter: Incremented for each multicast good frame of lengths smaller than 1518 (non VLAN) or 1522 (VLAN) excluding the broadcast frames. This does not include range, length errors. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:22] | Reserved | 0x0 | Reserved |
| [21:0] | RBCA | 0x0 | Receive broadcast packet counter: Incremented for each broadcast good frame of lengths smaller than 1518 (non VLAN) or 1522 (VLAN) excluding the multicast frames. This does not look at range/length errors. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:18] | Reserved | 0x0 | Reserved |
| [17:0] | RXCF | 0x0 | Receive control frame packet counter: Incremented for each MAC control frame received (PAUSE and Unsupported). |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:12] | Reserved | 0x0 | Reserved |
| [11:0] | RXPF | 0x0 | Receive PAUSE frame packet counter: Incremented each time a valid PAUSE MAC control frame is received. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:12] | Reserved | 0x0 | Reserved |
| [11:0] | RXUO | 0x0 | Receive unknown OP-code counter: Incremented each time a MAC control frame containing an op-code other than a PAUSE is received. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:12] | Reserved | 0x0 | Reserved |
| [11:0] | RALN | 0x0 | Receive alignment error counter: Incremented for each received frame from 64 to 1518.This contains an invalid FCS and is not an integral number of bytes. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:16] | Reserved | 0x0 | Reserved |
| [15:0] | RFLR | 0x0 | Receive frame length error counter: Incremented for each frame received in which the 802.3 length field does not match with the number of the data bytes actually received (46-1500 bytes). The counter is not incremented if the length field is not a valid 802.3 length. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:12] | Reserved | 0x0 | Reserved |
| [11:0] | RCDE | 0x0 | Receive code error counter: Incremented each time a valid carrier is present and at least one invalid data symbol is detected. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:12] | Reserved | 0x0 | Reserved |
| [11:0] | RCSE | 0x0 | Receive false carrier counter: Incremented each time a false carrier is detected during idle, as defined by a 1 on RX_ER, and an ‘0xE’ on RXD. The event is reported along with the statistics generated on the next received frame. Only one false carrier condition can be detected and logged between frames. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:12] | Reserved | 0x0 | Reserved |
| [11:0] | RUND | 0x0 | Receive undersize packet counter: Incremented each time a frame is received which is less than 64 bytes in length and contains a valid FCS. This does not include range, length errors. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:12] | Reserved | 0x0 | Reserved |
| [11:0] | ROVR | 0x0 | Receive oversize packet counter: Incremented each time a frame is received which exceeded 1518 (non VLAN) or 1522 (VLAN) and contains a valid FCS. This does not include range, length errors. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:12] | Reserved | 0x0 | Reserved |
| [11:0] | RFRG | 0x0 | Receive fragments counter: Incremented for each frame received which is less than 64 bytes in length and contains an invalid FCS. The received frame includes integral and non-integral lengths. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:12] | Reserved | 0x0 | Reserved |
| [11:0] | Reserved | 0x0 | Receive jabber counter: Incremented for frames received which exceed 1518 (non VLAN) or 1522 (VLAN) bytes and contains an invalid FCS. The received frame, includes alignment errors. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:12] | Reserved | 0x0 | Reserved |
| [11:0] | RDRP | 0x0 | Receive dropped packets counter: Incremented for frames received which are streamed to system but are later dropped due to lack of system resources. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:24] | Reserved | 0x0 | Reserved |
| [23:0] | TPKT | 0x0 | Transmit byte counter: Incremented by the number of bytes that are transmitted including fragments of frames, which are involved in collisions. This count does not include preamble/SFD or jam bytes. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:18] | Reserved | 0x0 | Reserved |
| [17:0] | TPKT | 0x0 | Transmit packet counter: Incremented for each transmitted packet (including bad packets, excessive deferred packets, excessive collision packets, late collision packets, all unicast, broadcast, and multicast packets). |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:18] | Reserved | 0x0 | Reserved |
| [17:0] | TPKT | 0x0 | Transmit packet counter: Incremented for each transmitted packet (including bad packets, excessive deferred packets, excessive collision packets, late collision packets, all unicast, broadcast, and multicast packets). |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:18] | Reserved | 0x0 | Reserved |
| [17:0] | TBCA | 0x0 | Transmit broadcast packet counter: Incremented for each broadcast frame transmitted (excluding multicast frames). |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:12] | Reserved | 0x0 | Reserved |
| [11:0] | TXPF | 0x0 | Transmit PAUSE frame packet counter: Incremented each time a valid PAUSE MAC control frame is transmitted. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:12] | Reserved | 0x0 | Reserved |
| [11:0] | TDFR | 0x0 | Transmit deferral packet counter: Incremented for each frame, which is deferred on its first transmission attempt. This does not include frames involved in collisions. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:12] | Reserved | 0x0 | Reserved |
| [11:0] | TEDF | 0x0 | Transmit excessive deferral packet counter: Incremented for aborted frames which are deferred for an excessive period of time (3036 byte times). |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:12] | Reserved | 0x0 | Reserved |
| [11:0] | TSCL | 0x0 | Transmit single collision packet counter: Incremented for each transmitted frame which experiences exactly one collision during the transmission. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:12] | Reserved | 0x0 | Reserved |
| [11:0] | TMCL | 0x0 | Transmit multiple collision packet counter: Incremented for each transmitted frame which experiences 2-15 collisions (including any late collisions). |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:12] | Reserved | 0x0 | Reserved |
| [11:0] | TLCL | 0x0 | Transmit late collision packet counter: Incremented for each transmitted frame which experiences a late collision during a transmission attempt. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:12] | Reserved | 0x0 | Reserved |
| [11:0] | TXCL | 0x0 | Transmit excessive collision packet counter: Incremented for each frame that experiences 16 collisions during the transmission and is aborted. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:13] | Reserved | 0x0 | Reserved |
| [12:0] | TNCL | 0X0 | Transmit total collision counter: Incremented by the number of collisions experienced during the transmission of a frame due to simultaneous transmitting and receiving. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:12] | Reserved | 0x0 | Reserved |
| [11:0] | TPFH | 0x0 | Transmit PAUSE frames honored counter: Incremented each time a valid PAUSE MAC control frame is transmitted and honored. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:12] | Reserved | 0x0 | Reserved |
| [11:0] | TDRP | 0x0 | Transmit drop frame counter: Incremented each time the transmit PAUSE frame honored input to PE-MSTAT is asserted. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:12] | Reserved | 0x0 | Reserved |
| [11:0] | TJBR | 0x0 | Transmit jabber frame counter: Incremented for each oversized transmitted frame with an incorrect FCS value. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:12] | Reserved | 0x0 | Reserved |
| [11:0] | TFCS | 0x0 | Transmit FCS error counter: Incremented for each valid sized packet with an incorrect FCS value. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:12] | Reserved | 0x0 | Reserved |
| [11:0] | TXCS | 0x0 | Transmit control frame counter: Incremented for each valid size frame with a type field signifying a control frame. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:12] | Reserved | 0x0 | Reserved |
| [11:0] | TOVR | 0x0 | Transmit oversize frame counter: Incremented for each oversized transmitted frame with a correct FCS value. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:12] | Reserved | 0x0 | Reserved |
| [11:0] | TUND | 0x0 | Transmit undersize frame counter: Incremented for each frame less than 64 bytes, with a correct FCS value. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:12] | Reserved | 0x0 | Reserved |
| [11:0] | TFRG | 0x0 | Transmit fragment counter: Incremented for each frame less than 64 bytes, with an incorrect FCS value. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| 31 | C164 | 0x0 | Carry register 1 TR64 counter carry bit |
| 30 | C1127 | 0x0 | Carry register 1 TR127 counter carry bit |
| 29 | C1255 | 0x0 | Carry register 1 TR255 counter carry bit |
| 28 | C1511 | 0x0 | Carry register 1 TR511 counter carry bit |
| 27 | C11k | 0x0 | Carry register 1 TR1K counter carry bit |
| 26 | C1MAX | 0x0 | Carry register 1 TRMAX counter carry bit |
| 25 | C1MGV | 0x0 | Carry register 1 TRMGV counter carry bit |
| [24:17] | Reserved | 0x0 | Reserved |
| 16 | C1RBY | 0x0 | Carry register 1 RBYT counter carry bit |
| 15 | C1RPK | 0x0 | Carry register 1 RPKT counter carry bit |
| 14 | C1RFC | 0x0 | Carry register 1 RFCS counter carry bit |
| 13 | C1RMC | 0x0 | Carry register 1 RMCA counter carry bit |
| 12 | C1RBC | 0x0 | Carry register 1 RBCA counter carry bit |
| 11 | C1RXC | 0x0 | Carry register 1 RXCF counter carry bit |
| 10 | C1RXP | 0x0 | Carry register 1 RXPF counter carry bit |
| 9 | C1RXU | 0x0 | Carry register 1 RXUO counter carry bit |
| 8 | C1RAL | 0x0 | Carry register 1 RALN counter carry bit |
| 7 | C1RFL | 0x0 | Carry register 1 RFLR counter carry bit |
| 6 | C1RCD | 0x0 | Carry register 1 RCDE counter carry bit |
| 5 | C1RCS | 0x0 | Carry register 1 RCSE counter carry bit |
| 4 | C1RUN | 0x0 | Carry register 1 RUND counter carry bit |
| 3 | C1ROV | 0x0 | Carry register 1 ROVR counter carry bit |
| 2 | C1RFR | 0x0 | Carry register 1 RFRG counter carry bit |
| 1 | C1RJB | 0x0 | Carry register 1 RJBR counter carry bit |
| 0 | C1RDR | 0x0 | Carry register 1 RDRP counter carry bit |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:20] | Reserved | 0x0 | Reserved |
| 19 | C2TJB | 0x0 | Carry register 2 TJBR counter carry bit |
| 18 | C2TFC | 0x0 | Carry register 2 TXFC counter carry bit |
| 17 | C2TCF | 0x0 | Carry register 2 TXCF counter carry bit |
| 16 | C2TOV | 0x0 | Carry register 2 TOVR counter carry bit |
| 15 | C2TUN | 0x0 | Carry register 2 TUND counter carry bit |
| 14 | C2TFG | 0x0 | Carry register 2 TFRG counter carry bit |
| 13 | C2TBY | 0x0 | Carry register 2 TBYT counter carry bit |
| 12 | C2TPK | 0x0 | Carry register 2 TPKT counter carry bit |
| 11 | C2TMC | 0x0 | Carry register 2 TMCA counter carry bit |
| 10 | C2TBC | 0x0 | Carry register 2 TBCA counter carry bit |
| 9 | C2TPF | 0x0 | Carry register 2 TXPF counter carry bit |
| 8 | C2TDF | 0x0 | Carry register 2 TDFR counter carry bit |
| 7 | C2TED | 0x0 | Carry register 2 TEDF counter carry bit |
| 6 | C2TSC | 0x0 | Carry register 2 TSCL counter carry bit |
| 5 | C2TMA | 0x0 | Carry register 2 TMCL counter carry bit |
| 4 | C2TLC | 0x0 | Carry register 2 TLCL counter carry bit |
| 3 | C2TXC | 0x0 | Carry register 2 TXCL counter carry bit |
| 2 | C2TNC | 0x0 | Carry register 2 TNCL counter carry bit |
| 1 | C2TPH | 0x0 | Carry register 2 TPFH counter carry bit |
| 0 | C2TDP | 0x0 | Carry register 2 TDRP counter carry bit |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| 31 | M164 | 0x1 | Mask register 1 TR64 counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| 30 | M1127 | 0x1 | Mask register 1 TR127 counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| 29 | M1255 | 0x1 | Mask register 1 TR255 counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| 28 | M1511 | 0x1 | Mask register 1 TR511 counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| 27 | M11k | 0x1 | Mask register 1 TR1K counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| 26 | M1MAX | 0x1 | Mask register 1 TRMAX counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| 25 | M1MGV | 0x1 | Mask register 1 TRMGV counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| [24:17] | Reserved | 0x0 | Reserved |
| 16 | M1RBY | 0x1 | Mask register 1 RBYT counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| 15 | M1RPK | 0x1 | Mask register 1 RPKT counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| 14 | M1RFC | 0x1 | Mask register 1 RFCS counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| 13 | M1RMC | 0x1 | Mask register 1 RMCA counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| 12 | M1RBC | 0x1 | Mask register 1 RBCA counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| 11 | M1RXC | 0x1 | Mask register 1 RXCF counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| 10 | M1RXP | 0x1 | Mask register 1 RXPF counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| 9 | M1RXU | 0x1 | Mask register 1 RXUO counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| 8 | M1RAL | 0x1 | Mask register 1 RALN counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| 7 | M1RFL | 0x1 | Mask register 1 RFLR counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| 6 | M1RCD | 0x1 | Mask register 1 RCDE counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| 5 | M1RCS | 0x1 | Mask register 1 RCSE counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| 4 | M1 RUN | 0x1 | Mask register 1 RUND counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| 3 | M1ROV | 0x1 | Mask register 1 ROVR counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| 2 | M1RFR | 0x1 | Mask register 1 RFRG counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| 1 | M1RJB | 0x1 | Mask register 1 RJBR counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| 0 | M1RDR | 0x1 | Mask register 1 RDRP counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [31:20] | Reserved | 0x0 | Reserved |
| 19 | M2TJB | 0x1 | Mask register 2 TJBR counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| 18 | M2TFC | 0x1 | Mask register 2 TXFC counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| 17 | M2TCF | 0x1 | Mask register 2 TXCF counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| 16 | M2TOV | 0x1 | Mask register 2 TOVR counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| 15 | M2TUN | 0x1 | Mask register 2 TUND counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| 14 | M2TFG | 0x1 | Mask register 2 TFRG counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| 13 | M2TBY | 0x1 | Mask register 2 TBYT counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| 12 | M2TPK | 0x1 | Mask register 2 TPKT counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| 11 | M2TMC | 0x1 | Mask register 2 TMCA counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| 10 | M2TBC | 0x1 | Mask register 2 TBCA counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| 9 | M2TPF | 0x1 | Mask register 2 TXPF counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| 8 | M2TDF | 0x1 | Mask register 2 TDFR counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| 7 | M2TED | 0x1 | Mask register 2 TEDF counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| 6 | M2TSC | 0x1 | Mask register 2 TSCL counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| 5 | M2TMA | 0x1 | Mask register 2 TMCL counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| 4 | M2TLC | 0x1 | Mask register 2 TLCL counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| 3 | M2TXC | 0x1 | Mask register 2 TXCL counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| 2 | M2TNC | 0x1 | Mask register 2 TNCL counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| 1 | M2TPH | 0x1 | Mask register 2 TPFH counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| 0 | M2TDP | 0x1 | Mask register 2 TDRP counter carry bit 0: Unmask the counter carry bit 1: Mask the counter carry bit |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| 15 | PHY RESET | 0x0 | Setting this bit causes the PETEX, PEREX, and PEANX sub-modules in the M-SGMII core to be reset. This bit is self-clearing. |
| 14 | LOOP BACK | 0x0 | Setting this bit causes the M-SGMII loopback. Clearing this bit results in normal operation. |
| 13 | Reserved | 0x0 | Reserved |
| 12 | AUTO-NEGOTIATION ENABLE | 0x0 | Setting this bit enables the auto-negotiation process. |
| [11:10] | Reserved | 0x0 | Reserved |
| 9 | RESET AUTO-NEGOTIATION | 0x0 | Setting this bit causes the auto-negotiation process to restart. This action is only available when auto-negotiation has been enabled. |
| [8:0] | Reserved | 0x0 | Reserved |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [15:9] | Reserved | 0x0 | Reserved |
| 8 | EXTENDED STATUS | 0x0 | This bit returns “1” on read to indicate that the PHY status information is also contained in EXTENDED STATUS register. |
| 7 | Reserved | 0x0 | Reserved |
| 6 | MF PREMABLE SUPPRESSION ENABLE | 0x0 | This bit indicates whether the PHY is capable
of handling MII management frames without the 32-bit preamble field. Returns “1” on read to indicate the support for suppressed preamble MII management frames. |
| 5 | AUTO-NEGOTIATION COMPLETE | 0x0 | This bit indicates that the auto-negotiation process is completed. Returns “0” on read when either the auto-negotiation process is underway or when the auto-negotiation function is disabled. |
| 4 | REMOTE FAULT | 0x0 | This bit returns “1” on read to indicate a remote fault condition has been detected between the M-SGMII and the PHY. This bit latches high in order for software to detect the condition. Each read of the STATUS register clears this bit. |
| 3 | AUTO-NEGOTIATION ABILITY | 0x0 | When “1”, this bit indicates that the M-SGMII has the ability to perform auto-negotiation. Returns “1” on read. |
| 2 | LINK STATUS | This bit indicates that a valid link is
established between the
M-SGMII and the PHY. Returns “0” on read to indicate that there is no valid link is established. This bit latches low to allow software polling to detect a failure condition. | |
| 1 | Reserved | 0x0 | Reserved |
| 0 | EXTENDED CAPABILITY | 0x1 | This bit returns “1” on read to indicates that the M-SGMII contains the extended set of registers (those beyond CONTROL and STATUS). |
| Bit Number | Name | Reset Value | Description | ||
|---|---|---|---|---|---|
| 15 | LINK UP | 0x0 | Assertion of this bit indicates that the link between M-SGMII and PHY is up. | ||
| [14:13] | Reserved | 0x0 | Reserved | ||
| 12 | FULL DUPLEX | 0x0 | Assertion of this bit indicates that the link between M-SGMII and PHY is up and transferring data in full-duplex mode. | ||
| [11:10] | LINK SPEED | 0x0 | Assertion of these two bits indicate that the link between M-SGMII and PHY is up. The following table shows the speed at which the link is transferring data: | ||
| LINK SPEED [11] | LINK SPEED [10] | Capability | |||
| 1 | 1 | Reserved | |||
| 1 | 0 | 1000 Mbps | |||
| 0 | 1 | 100 Mbps | |||
| 0 | 0 | 10 Mbps | |||
| [9:0] | Reserved | 0x0 | These bits must always be written ‘0000000001’ for correct M-SGMII operation. | ||
| Bit Number | Name | Reset Value | Description | ||
|---|---|---|---|---|---|
| 15 | LINK UP | 0x0 | When the M-SGMII is integrated to a MAC, such as the PE-MCXMAC, and is communicating with another SGMII PHY module, assertion of this bit indicates that the link is up. When the M-SGMII is integrated to a PHY and is not integrated to MAC, this bit is invalid. | ||
| [14:13] | Reserved | 0x0 | Reserved | ||
| 12 | FULL DUPLEX | 0x0 | Assertion of this bit indicates that LINK UP bit of the AN SGMII partner base page ability register is asserted and the link is transfers data in full-duplex mode. | ||
| [11:10] | LINK SPEED | 0x0 | Indicates the speed of the link as mentioned in the following table when LINK UP bit of the AN SGMII partner base page ability register is asserted. | ||
| LINK SPEED [11] | LINK SPEED [10] | Capability | |||
| 1 | 1 | Reserved | |||
| 1 | 0 | 1000 Mbps | |||
| 0 | 1 | 100 Mbps | |||
| 0 | 0 | 10 Mbps | |||
| [9:0] | Reserved | 0x0 | Reserved | ||
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| [15:3] | Reserved | 0x0 | Reserved |
| 2 | NEXT PAGE ABLE | 0x0 | Returns “1” on read to indicate that the local device supports the next page function. |
| 1 | PAGE RECEIVED | 0x0 | Returns “1” on read to indicate that a new page has been received and stored in the applicable Table 10-109 or Table 10-111 register. This bit latches High for detection by software when polling. The bit is cleared on a read to the register. |
| 0 | Reserved | 0x0 | Reserved |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| 15 | NEXT PAGE | 0x0 | Assert this bit to indicate additional Next Pages to follow. Clear the bit to indicate the last page. |
| 14 | Reserved | 0x0 | Reserved |
| 13 | MESSAGE PAGE | 0x0 | Assert this bit to indicate a Message Page. Clear the bit to indicate an Unformatted Page. |
| 12 | ACKNOWLEDGE 2 | 0x0 | Used by the Next Page function to indicate that the device has the ability to comply with the message. Assert this bit if the local device will comply with the message. Clear the bit if the local device cannot comply with message. |
| 11 | TOGGLE | 0x0 | This bit is read only. Used to ensure synchronization with the Link Partner during Next Page exchange. This bit always takes the opposite value to the toggle bit of the previously exchanged Link Code Word. The initial value in the first Next Page transmitted is the inverse of bit 11 in the base Link Code Word. |
| [10:0] | MESSAGE / UNFORMATTED CODE FIELD | 0x0 | Message pages are formatted pages that carry a predefined Message Code, which is enumerated in IEEE 802.3u/Annex 28C. Unformatted code fields take an arbitrary value. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| 15 | NEXT PAGE | The link partner asserts this bit to indicate additional Next Pages to follow. When “0”, indicates last Next Page from link partner. | |
| 14 | Reserved | Reserved | |
| 13 | MESSAGE PAGE | When “1”, indicates Message Page. When “0”, indicates Unformatted Page. | |
| 12 | ACKNOWLEDGE 2 | Indicates link partner’s ability to comply
with the message. When “1”, link partner complies with message. When “0”, link partner cannot comply with message. | |
| 11 | TOGGLE | Used to ensure synchronization with the link partner during next page exchange. This bit always takes the opposite value to the toggle bit of the previously exchanged link code word. The initial value in the first next page transmitted is the inverse of bit 11 in the base link code word. | |
| [10:0] | MESSAGE / UNFORMATTED CODE FIELD | Message pages are formatted pages that carry a predefined message code, which is enumerated in the IEEE 802.3u/Annex 28C. Unformatted code fields take an arbitrary value. |
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| 15 | 1000BASE-X FULL-DUPLEX | 0x1 | When “1”, indicates that the PHY can operate in 1000BASE-X full-duplex mode. When “0”, indicates that the PHY cannot operate in 1000BASE-X full-duplex mode. |
| 14 | 1000BASE-X HALF-DUPLEX | 0x0 | When “1”, indicates that the PHY can operate in 1000BASE-X half-duplex mode. When “0”, indicates that the PHY cannot operate in 1000BASE-X half-duplex mode. |
| 13 | 1000BASE-T FULL-DUPLEX | 0x1 | When “1”, indicates that the PHY can operate in 1000BASE-T full-duplex mode. When “0”, indicates that the PHY cannot operate in 1000BASE-T full-duplex mode. Returns “1” on read. |
| 12 | 1000BASE-T HALF-DUPLEX | 0x0 | When “1”, indicates that the PHY can operate in 1000BASE-T half-duplex mode. When “0”, indicates PHY cannot operate in 1000BASE-T half-duplex mode. |
| [11:0] | Reserved | 0x0 | Reserved |
| Bit Number | Name | Reset Value | Description | |||
|---|---|---|---|---|---|---|
| 15 | JITTER DIAGNOSTIC ENABLE | 0x0 | Set this bit to enable the M-SGMII to transmit the jitter test patterns defined in IEEE 802.3z 36A. Clear this bit to enable normal transmit operation. | |||
| [14:12] | JITTER PATTERN SELECT | 0x0 | Selects the jitter pattern to be transmitted in Diagnostics mode. Encoding of this field is as follows: | |||
| Jitter Pattern Select | Bit 14 | Bit 13 | Bit 12 | |||
| User defined custom pattern | 0 | 0 | 0 | |||
| Annex 36A defined high frequency | 0 | 0 | 1 | |||
| Annex 36A defined mixed frequency | 0 | 1 | 0 | |||
| Custom defined low frequency | 0 | 1 | 1 | |||
| Random jitter pattern | 1 | 0 | 0 | |||
| Annex 36A defined low frequency | 1 | 0 | 1 | |||
| Reserved | 1 | 1 | 0 | |||
| Reserved | 1 | 1 | 1 | |||
| [11:10] | Reserved | 0x0 | Reserved | |||
| [9:0] | CUSTOM JITTER PATTERN | 0x0 | Used in conjunction with JITTER PATTERN SELECT and JITTER DIAGNOSTIC ENABLE. Set this field to the desired custom pattern, which is transmitted continuously. | |||
| Bit Number | Name | Reset Value | Description |
|---|---|---|---|
| 15 | SOFT RESET | 0x0 | This bit resets the functional modules in the M-SGMII. Clear it for normal operation. Its default is “0”. |
| 14 | SHORTCUT LINK TIMER | 0x0 | Set this bit to reduce the amount of
simulation time needed to time the 1.6 ms Link Timer. Clear it for normal operation. |
| 13 | DISABLE RECEIVE RUNNING DISPARITY | 0x0 | Set this bit to disable the running disparity calculation and checking in the receive direction. This bit must be “0” for correct M-SGMII operation. |
| 12 | DISABLE TRANSMIT RUNNING DISPARITY | 0x0 | Set this bit to disable the running disparity calculation and checking in the transmit direction. This bit must be “0” for correct M-SGMI operation. |
| [11:9] | Reserved | 0x0 | Reserved |
| 8 | AUTO-NEGOTIATION SENSE | 0x0 | Set this bit to allow the auto-negotiation for 1000BASE-X, which is used to exchange information between link partners. Clear this bit when IEEE 802.3z Clause 37 behavior is desired, which results in the link not coming up. |
| [7:6] | Reserved | 0x0 | Reserved |
| 5 | RECEIVE CLOCK SELECT | 0x0 | Set this bit to configure the M-SGMII to
accept a 125 MHz receive clock from the SerDes PHY. Clear this bit to allow the M-SGMII to accept dual split-phase 62.5 MHz receive clocks. This bit must be “0” for correct M-SGMII operation. |
| 4 | GMII MODE | 0x0 | When cleared, this bit defines the M-SGMII as being in 1000BASE-X SerDes mode. This bit must be “0” for correct M-SGMII operation. |
| [3:2] | Reserved | 0x0 | Reserved |
| 1 | ENABLE WRAP | 0x0 | Set this bit to configure the SerDes in Loopback mode. Clear this bit to permit normal operation. |
| 0 | ENABLE COMMA DETECT | 0x0 | Set this bit to allow the SerDes PHY to perform code group alignment based upon the detection of a comma. |