9.15.10.56 Example

The following example sets the IR length to '2' for the non-Actel device 'MyDevice4':

set_device_ir –name {MyDevice4} –ir {2}

set_device_name

Changes the user name of a device in the chain. Chain programming mode must be set .

set_device_name -name {name} -new_name {new_name}