9.15.10.12 Example
save_log
The following example runs the selected actionS on the programmers 'FP30085' and 'FP30086'.
run_selected_actions –name {FP300085} –name {FP300086}
Example using return code:
if {[catch {run_selected_actions} return_val]} {puts "Error running Action"} else {puts "exit code $return_val"}
Example returning exit code to the command line (returns exit 99 on script failure, otherwise returns exit code from selected action):
if {[catch {run_selected_actions} return_val]}{exit 99} else {exit $return_val}
Saves the log file.
save_log -file {file}