9.15.10.64 Example

The following example sets the device order for 'MyDevice1', 'MyDevice2', 'MyDevice3', and 'MyDevice4'. 'MyDevice2' is unspecified so it moves to the end of the chain.

set_device_order –name {MyDevice3} –name {MyDevice1} –name {MyDevice4}

the new order is:

MyDevice3 MyDevice1 MyDevice4 MyDevice2

set_device_tck

set_device_tck -name {name} -tck {tck}

Sets the maximum TCK frequency of a non-Actel device in the chain. Chain programming mode must be set. The device must be a non-Actel device.