9.15.10.60 Example

The following example changes the user name of the device from 'MyDevice4' to 'MyDevice5':

set_device_name –name {MyDevice4} –new_name {MyDevice5}

set_device_order

set_device_order (-name {name})*

Sets the order of the devices in the chain to the order specified. Chain programming mode must have been set. Unspecified devices will be at the end of the chain.