9.15.10.48 Example

The following example identifies the device 'A3P250' for debugging:

set_debug_device –name {A3P250}

set_debug_programmer

set_debug_programmer -name {programmer_name}

Identifies the programmer you want to use for debugging (if you have more than one). The name of the programmer is the serial number on the bar code label on the FlashPro programmer.