9.15.10.68 Example
The following example sets the maximum TCK frequency of the non-Actel device 'MyDevice4':
set_device_tck –name {MyDevice4} –tck {2.25}
set_device_type
set_device_type -name {name} -type {type}
Changes the family of an Actel device in the chain. The device must be an Actel device. The device parameter below is now optional.