9.15.10.36 Example

The following examples runs the self test on the programmer '30175':

self_test_prg (-name {30175})*

set_bsdl_file

set_bsdl_file -name {name} -file {file}

Sets a BSDL file to a non-Actel device in the chain. Chain programming mode must have been set. The device must be a non-Actel device.