9.15.10.52 Example

The following example selects the programmer 10841

set_debug_programmer -name {10841}

set_device_ir

set_device_ir -name {name} -ir {ir}

Sets the IR length of a non-Actel device in the chain. Chain programming mode must be set. The device must be a non-Actel device.