2.2.26.2 INTEL-HEX
Industry standard file. Extensions are HEX and IHX. For example, file2.hex or file3.ihx.
A standard format created by Intel. Memory contents are stored in ASCII files using hexadecimal characters. Each file contains a series of records (lines of text) delimited by new line, ‘\n’, characters and each record starts with a ‘:’ character. For more information regarding this format, refer to the Intel-Hex Record Format Specification document available on the web (search Intel Hexadecimal Object File for several examples).
The Intel Hex Record is composed of five fields and arranged as follows:
:llaaaatt[dd...]cc
Where:
- ‘:’ : Is the start code of every Intel Hex record
- ‘ll’ : Is the byte count of the data field
- ‘aaaa’ : Is the 16-bit address of the beginning of the memory position for the data. Address is big endian.
- ‘tt’ : Is record type, defines the data field.
- 00 : data record
- 01 : end of file record
- 02 : extended segment address record
- 03 : start segment address record ( ignored by Actel tools )
- 04 : extended linear address record
- 05 : start linear address record ( ignored by Actel tools )
- ‘[dd...]’ is a sequence of n bytes of the data; n is equivalent to what was specified in the ll field.
- ‘cc’ : Is a checksum of count, address, and data
Example Intel Hex Record:
:10000000112233445566778899FFFA
Where 11 is the LSB and FF is the MSB.