20.2.8 SmartPower Standard Toolbar and Menu Commands

The SmartPower standard toolbar contains commands for performing common SmartPower operations on your designs. Roll the mouse pointer over the toolbar button to view a description of the button. Click the button to access the command.

Table 20-3.  SmartPower Toolbar

Toolbar Button

Description

Commit

þÿ

Settings Summary

þÿ

Operating Conditions

þÿ

Options

þÿ

Export Path Grid

þÿ

Copy Path Grid

þÿ

Print Grid

Generate Power Report

Table 20-4.  SmartPower Toolbar

Toolbar Button

Description

þÿ

Initialize Frequencies and Probabilities

þÿ

Refreshes Vectorless Estimation

The PC and UNIX workstation versions of SmartPower have the same menus. However, some dialog boxes may look slightly different on the two platforms due to the different window environments. The functionality is the same on both platforms, though the locations of the fields and buttons on the dialog boxes may vary. The names of some fields may also vary between the PC and workstation versions.

File Menu

Table 20-5. File Menu

Menu

Description

Commit

Commits power information to Designer. You must commit your changes if you wish to save your settings in SmartPower. If you commit your changes, the information is stored in the .adb file, and your settings are restored the next time you open your design in SmartPower

Export Grid

Exports the selected area of the Report window to a text (.txt) file

Print Grid

Prints the selected area of the Report window

Settings Summary

Displays a summary of the power settings for the current design

Close

Closes SmartPower

Table 20-6. Edit Menu

Menu

Sub-Menu

Description

Domains

New Clock Domain

Adds a clock domain

New Set of Pins

Adds a set of pins

Delete Domain

Deletes a clock domain

Edit Domain

Edits a clock domain

Table 20-7. Edit Menu

Menu

Sub-Menu

Description

Modes and Scenarios

Use for Analysis > mode or scenario name

Sets the selected mode or scenario to be used for analysis

Use for PDPR > mode or scenario name

Sets the selected mode or scenario to be used for Power-Driven Layout

Custom Modes > New Custom Mode

Creates a new custom mode

Custom Modes > Edit Custom Mode

Edits a custom mode

Custom Modes > Delete Custom Mode

Deletes a custom mode

Custom Scenarios > New Scenario

Creates a new custom scenario

Custom Scenarios > Edit Scenario

Edits a custom scenario

Custom Scenarios > Delete Scenario

Deletes a custom scenario

Copy Grid

—

Copies the selected cells of the dynamic grid onto the clipboard

Table 20-8. View Menu

Menu

Description

Standard Toolbar

Displays or hides the SmartPower Standard toolbar

Preferences Toolbar

Displays or hides the SmartPower Preferences toolbar

Modes and Scenarios Toolbar

Displays or hides the Modes and Scenarios toolbar

Unprocessed Simulation Files Toolbar

Displays or hides the Unprocessed Simulation Files toolbar

Table 20-9. View Menu

Menu

Description

Customize Columns

Selects and orders the columns displayed in the user interface

Reset Window Layout

Resets the window layout to the default layout

Table 20-10. Tools Menu

Menu

Sub-Menu

Description

Initialize Frequencies and Probabilities

—

Imports clock constraints from SmartTime and enables the user to input frequencies and probabilities for the design

Operating Conditions

—

Enables the user to customize the operating conditions used in SmartPower

Options

—

Invokes the Options dialog box, where you can set analysis and display preferences

Reports

Power Report

Generates a power report

Scenario Power Report

Generates a scenario power report

Cycle Accurate Power Report

Generates a cycle accurate power report

Activity and Hazards Power Report

Generates an activity and hazards power report

Cycle Accurate Power Analysis

—

Generates a cycle-accurate power analysis

Table 20-11. Simulation Menu

Menu

Description

Import VCD File

Invokes the Import VCD Options dialog box

Remove VCD file

Removes the selected CVD file from the design

Audit files

Audits simulation files within the project

Table 20-12. Help Menu

Menu

Description

Help on current tab

Displays the help content for the current tab

Help Topics

Opens the help files for SmartPower

SmartPower User's Guide

Displays the SmartPower User's Guide

Data Change History

Displays the data change history report