20.2.22 Removing a VCD File

The Value Change Dump (VCD) file is a simulation file. The format of this file is specified in the IEEE 1364 standard.

To remove a VCD file:

  • Select the VCD file from Active mode or a custom mode, right-click the VCD file, and select Remove VCD File from <mode name> Mode; or
  • From the Simulation menu, select Remove VCD File > <file name>

Any annotation will be removed when you remove the VCD file.