21.6.7 Viewing External Setup Paths

To view External Setup paths, click External Setup in the Domain Browser to display the external setup timing (as shown in the following figure). Note that the slack is positive in the tutorial example, indicating there are no timing violations.
Figure 21-13. SmartTime External Setup Path List
þÿ