9.22.18.3 Selecting Action and Procedures

You can select actions from the Basic mode and the Advanced mode. The Basic mode is provided for users that only require the Program, Verify and Erase actions. In Basic mode, other actions are not visible, and the Procedures run by an Action cannot be modified.
Figure 9-169. Basic Mode
???

The Advanced mode enables you to select an action and modify the procedures for the selected action. In Advanced mode, actions are determined by the stapl standard used.

Figure 9-170. Advanced Mode
???

To select an action (Advanced Mode):

  1. Click the down arrow in the Action menu and select and action.
    Figure 9-171. Action Menu
    ???
  2. Click the Procedures button. The Select Action and Procedures dialog box appears.
    Figure 9-172. Select Action And Procedures Dialog Box
    ???
  3. Select a procedure or click the Restore Default Procedures button. Gray checkboxes indicate that the procedure is mandatory.
    Note: The procedures in the Select Action And Procedures dialog box are determined by the STAPL standard. The Recommended procedures are selected by default and the Optional procedures are unselected by default.
  4. Click OK.
Note: You can also click the Select Action and Procedures dialog box from the toolbar.