1.2.13 ASB Advanced Options - SMEV Status

This option exposes status signals from the SMEV; these are useful for monitoring the current processing state of the SMEV.

The following table displays the exposed SMEV Status ports:

Port NameInput/OutputDescription
EV_DONEOutputSMEV Done – Indicates that the SMEV is done for the current channel.
EV_EVFLAGOutputSMEV Active – Indicates that the SMEV is currently in effect for the channel that has just been sampled by the ASSC.
EV_CHHOLD[4:0]OutputChannel Value – The channel that the SMEV is currently processing