4.3.1.7 Reference Divider Synchronous Enable

Each CCC has an FPGA fabric input—REFCLK_SYNC_EN—to synchronously enable the RFDIV of both the PLLs. Internally, each PLL has its own enable for the RFDIV and is controlled through a PLL register map.

If the same reference clock is routed to both the PLLs in a CCC and needs to be divided, asserting REFCLK_SYNC_EN enables the reference divider of both PLLs on the same reference clock rising edge. This ensures proper alignment of the output edges from both PLLs, synchronized with the reference clock.

Note: This feature is not supported in the current version of Libero SoC.