1.2.5.1.26 TCPIP_MAC_Open Function
C
DRV_HANDLE TCPIP_MAC_Open(
const SYS_MODULE_INDEX drvIndex,
const DRV_IO_INTENT intent
);
Description
This is the function that opens an instance of the MAC. Once a MAC client handle is obtained all the MAC functions can be accessed using that handle.
Precondtions
TCPIP_MAC_Initialize() should have been called.
Parameters
| Parameters | Description |
|---|---|
| drvIndex | Identifier for the driver instance to be opened. |
| intent | Zero or more of the values from the enumeration DRV_IO_INTENT ORed together to indicate the intended use of the driver. |
Returns
Valid handle - if the open function succeeded.
DRV_HANDLE_INVALID - If an error occurs.
Remarks
The intent parameter is not used in the current implementation and is maintained only for compatibility with the generic driver Open function signature.