1.2.5.1.53 TCPIP_MAC_StatisticsGet Function
C
TCPIP_MAC_RES TCPIP_MAC_StatisticsGet(
DRV_HANDLE hMac,
TCPIP_MAC_RX_STATISTICS* pRxStatistics,
TCPIP_MAC_TX_STATISTICS* pTxStatistics
);
Description
This function will get the current value of the statistic counters maintained by the MAC driver.
Precondtions
TCPIP_MAC_Initialize() should have been called. TCPIP_MAC_Open() should have been called to obtain a valid handle.
Parameters
| Parameters | Description |
|---|---|
| hMac | Handle identifying the MAC driver client. |
| pRxStatistics | Pointer to a TCPIP_MAC_RX_STATISTICS that will receive the current RX statistics counters. Can be NULL if not needed. |
| pTxStatistics | Pointer to a TCPIP_MAC_TX_STATISTICS that will receive the current TX statistics counters. Can be NULL if not needed. |
Returns
TCPIP_MAC_RES_OK - If all processing went on OK.
TCPIP_MAC_RES_OP_ERR error code - If function not supported by the driver.
Remarks
The reported values are info only and change dynamically.