1.2.5.1.46 TCPIP_MAC_Reinitialize Function
C
void TCPIP_MAC_Reinitialize(
SYS_MODULE_OBJ object,
const SYS_MODULE_INIT * const init
);
Description
MAC Re-Initialize function. void TCPIP_MAC_Reinitialize(SYS_MODULE_OBJ object, const SYS_MODULE_INIT * const init);
This is the function that re-initializes the MAC. It is called by the stack as a result of the system changing power modes. Allows reinitialization of the MAC with different power modes, etc.
Precondtions
The TCPIP_MAC_Initialize() function should have been called.
Parameters
| Parameters | Description |
|---|---|
| object | Driver object handle, returned from TCPIP_MAC_Initialize(). |
| init | pointer to TCPIP_MAC_INIT initialization data containing: - macControl - Stack prepared data. - moduleData - Driver specific. Dependent on the MAC type. For PIC32 MAC driver, the TCPIP_MODULE_MAC_PIC32INT_CONFIG is used. |
Returns
None.
Remarks
This function is optional and is not currently implemented.