1.2.5.1.56 TCPIP_MAC_SynchReqF Type
C
typedef bool (* TCPIP_MAC_SynchReqF)(void* synchHandle, TCPIP_MAC_SYNCH_REQUEST request);
Description
Synchronization request Function: typedef bool (*TCPIP_MAC_SynchReqF)(void* synchHandle, TCPIP_MAC_SYNCH_REQUEST request);
This function describes the MAC synchronization request function. The MAC driver will call this function whenever it needs to create, delete, lock or unlock a synchronization object.
Members
| Members | Description |
|---|---|
| synchHandle | - Pointer to a valid storage area. - For TCPIP_MAC_SYNCH_REQUEST_OBJ_CREATE it is an address that will store a handle to identify the synchronization object to the OS (OSAL). - For other synchronization object request types the handle has to be valid and identify the synchronization object to the OS (OSAL). - For critical sections it maintains OS passed info. |
| request | A TCPIP_MAC_SYNCH_REQUEST type. |
Returns
True - If the call is successful.
False - If the call failed.
Remarks
None.