1.2.5.1.50 TCPIP_MAC_RxFilterHashTableEntrySet Function
C
TCPIP_MAC_RES TCPIP_MAC_RxFilterHashTableEntrySet(
DRV_HANDLE hMac,
const TCPIP_MAC_ADDR* DestMACAddr
);
Description
This function sets the MAC hash table filtering to allow packets sent to DestMACAddr to be received. It calculates a CRC-32 using polynomial 0x4C11DB7 over the 6 byte MAC address and then, using bits 28:23 of the CRC, will set the appropriate bits in the hash table filter registers.
The function will enable/disable the Hash Table receive filter if needed.
Precondtions
TCPIP_MAC_Initialize() should have been called. TCPIP_MAC_Open() should have been called to obtain a valid handle.
Parameters
| Parameters | Description |
|---|---|
| hMac | Handle identifying the MAC driver client. |
| DestMACAddr | Destination MAC address (6 bytes) to allow through the Hash Table Filter. If DestMACAddr is set to 00-00-00-00-00-00, then the hash table will be cleared of all entries and the filter will be disabled. |
Returns
TCPIP_MAC_RES_OK - If all processing went on OK.
TCPIP_MAC_RES error code - If function failed for some reason.
Remarks
There is no way to individually remove destination MAC addresses from the hash table since it is possible to have a hash collision and therefore multiple MAC addresses relying on the same hash table bit.
A workaround is to have the stack store each enabled MAC address and to perform the comparison at run time.
A call to TCPIP_MAC_RxFilterHashTableEntrySet() using a 00-00-00-00-00-00 destination MAC address, which will clear the entire hash table and disable the hash table filter. This will allow the receive of all packets, regardless of their destination.