1.2.5.1.59 TCPIP_MAC_TYPE Enumeration
C
typedef enum {
TCPIP_MAC_TYPE_NONE = 0,
TCPIP_MAC_TYPE_ETH,
TCPIP_MAC_TYPE_WLAN,
TCPIP_MAC_TYPES
} TCPIP_MAC_TYPE;
Description
MAC Types.
List of specific MAC types that indicate to the user of the MAC (TCP/IP stack) the actual type of the MAC driver.
Members
| Members | Description |
|---|---|
| TCPIP_MAC_TYPE_NONE = 0 | Invalid/unknown MAC type. |
| TCPIP_MAC_TYPE_ETH | Wired ethernet MAC type. |
| TCPIP_MAC_TYPE_WLAN | Wireless, Wi-Fi type MAC. |
| TCPIP_MAC_TYPES | Supported types. |
Remarks
Other types will be eventually added.