1.2.5.1.24 TCPIP_MAC_LinkCheck Function
C
bool TCPIP_MAC_LinkCheck(
DRV_HANDLE hMac
);
Description
This is a function that returns the current status of the link.
Precondtions
The TCPIP_MAC_Initialize() function should have been called. TCPIP_MAC_Open() should have been called to obtain a valid handle.
Parameters
| Parameters | Description |
|---|---|
| hMac | Handle identifying the MAC driver client. |
Returns
True - If the link is up.
False - If the link is down.
Remarks
The stack will call this function periodically. Therefore this function is not required to initiate a new PHY transaction and to wait for the result. It can just initiate a new PHY transaction and return immediately the result of the previous transaction.