1.2.5.1.57 TCPIP_MAC_Tasks Function
C
void TCPIP_MAC_Tasks(
SYS_MODULE_OBJ object
);
Description
This function is used to maintain the driver's internal state machine.
Precondtions
The TCPIP_MAC_Initialize() routine must have been called for the specified MAC driver instance.
Parameters
| Parameters | Description |
|---|---|
| object | Object handle for the specified driver instance (returned from TCPIP_MAC_Initialize()). |
Returns
None.
Remarks
This function is normally not called directly by an application. It is called by the system's Tasks routine (SYS_Tasks).
This function will never block or access any resources that may cause it to block.