1.2.5.1.7 TCPIP_MAC_Deinitialize Function
C
void TCPIP_MAC_Deinitialize(
SYS_MODULE_OBJ object
);
Description
MAC De-Initialize function. void TCPIP_MAC_Deinitialize(SYS_MODULE_OBJ object);
This is the function that deinitializes the MAC. It is called by the stack as a result of one interface going down.
Precondtions
TCPIP_MAC_Initialize() should have been called.
Parameters
| Parameters | Description |
|---|---|
| object | Driver object handle, returned from TCPIP_MAC_Initialize(). |
Returns
None.
Remarks
None.