1.2.5.1.25 TCPIP_MAC_MODULE_CTRL Structure
C
typedef struct {
TCPIP_MAC_HEAP_MallocF mallocF;
TCPIP_MAC_HEAP_CallocF callocF;
TCPIP_MAC_HEAP_FreeF freeF;
TCPIP_MAC_HEAP_HANDLE memH;
TCPIP_MAC_PKT_AllocF pktAllocF;
TCPIP_MAC_PKT_FreeF pktFreeF;
TCPIP_MAC_PKT_AckF pktAckF;
TCPIP_MAC_SynchReqF synchF;
TCPIP_MAC_EventF eventF;
const void* eventParam;
uint16_t nIfs;
uint16_t moduleId;
uint16_t netIx;
uint16_t segLoadOffset;
uint8_t macAction;
uint8_t powerMode;
TCPIP_MAC_ADDR ifPhyAddress;
} TCPIP_MAC_MODULE_CTRL;
Description
MAC Initialization Data.
This is the data structure that the MAC user (TCP/IP stack) passes on to the MAC driver at the MAC initialization time. It contains all the data needed for the MAC to initialize itself and to start processing packets.
Members
| Members | Description |
|---|---|
| mallocF | Malloc type allocation function. |
| callocF | Calloc type allocation function. |
| freeF | Free type allocation free function. |
| memH | Handle to be used in the stack allocation service calls. |
| pktAllocF | Packet allocation function. |
| pktFreeF | Packet free function. |
| pktAckF | Packet allocation function. |
| synchF | Synchronization object request function. |
| eventF | Event notification function. used by the MAC for event reporting. |
| eventParam | Parameter to be used when the event function is called. |
| nIfs | Number of the interfaces supported in this session. |
| moduleId | Module identifier. Allows multiple channels/ports, etc. MAC support. |
| netIx | Index of the current interface. |
| segLoadOffset | The extra space allocated at the beginning of the segment data buffer: TCPIP_MAC_DATA_SEGMENT.segLoad segLoadOffset == sizeof(TCPIP_MAC_SEGMENT_PAYLOAD::segmentPktPtr) + sizeof(TCPIP_MAC_SEGMENT_PAYLOAD::segmentDataGap). It can be different based on the MAC type included in the build MAC driver uses it to have the layout of the data segment. |
| macAction | Current action for the MAC/stack: TCPIP_MAC_ACTION value. |
| powerMode | The power mode for this interface to go to. Valid only if stackAction == init/reinit. Ignored for deinitialize operation. TCPIP_MAC_POWER_MODE value. |
| ifPhyAddress | Physical address of the interface. MAC sets this field as part of the initialization function. The stack will use this data as the interface address. |
Remarks
Most of the data that's passed in this structure is permanent data. It is maintained by the stack for one full session i.e., across Initialize() -> DeInitialize() calls.
Some fields are module specific though (like the memory allocation handle, allocation functions, etc.) that could be different from one module to the other.