BOOTSWP and Exceptions
Exceptions are not inhibited by the BOOTSWP instruction and will be handled in the same manner as they are for any two-cycle instruction. If an exception request be asserted at the CPU during the BOOTSWP (A stage), the instruction will be killed during exception processing. If the exception occurs after the BOOTSWP (A stage), the instruction will be allowed to complete during the first cycles of exception processing.