14.5.6.3 Wake-Up from Sleep
Figure 14-10 depicts how the CAN module will execute the SLEEP instruction and
how the module wakes up on bus activity. Upon a wake-up from Sleep mode, the WAKIF flag
is set.
The module will monitor the CAN receive line for activity while the module is sleeping. The device will generate a wake-up interrupt on the falling edges of CxRX if WAKIE is enabled.
The device will exit Sleep mode after a new mode request or a negative edge on CxRX.
The module will be in Sleep mode if either of the following is true:
- The system is in Sleep mode following Disable mode.
- The system is in Idle mode with SIDL =
1.
The module can be programmed to apply a low-pass filter function to the CAN receive input line while in Disable, Sleep or Idle mode. This feature can be used to protect the module from wake-up due to short glitches on the CAN bus lines. The WAKFIL bit (CxCON[8]) enables or disables the filter while the module is in Sleep.