3.6.8.11.4 FP Exception Masks
FSR bits INVAL, DIV0, OVF, UDF, INX, HUGI and SUBO have corresponding INVALM, DIV0M, OVFM, UDFM, INXM, HUGIM and SUBOM Exception Mask bits in the FCR. Should a “most-recent” exception flag be set by an operation, the corresponding Exception Mask bit in the FCR must already be clear in order to generate an interrupt.
Should an FCR Exception Mask bit be set when the corresponding FSR exception flag bit is set, no interrupt will be generated. In all cases (except SUBO which is an input operand exception), a default result (see Table 3-16) will be written. However, the corresponding “sticky” exception flag will be set and remain set until manually cleared.
| Instruction | Exceptions (FSR[6:0]) | Conditions | Default Results and Notes | ||||||
|---|---|---|---|---|---|---|---|---|---|
| SUBO | HUGI | INX | UDF | OVF | DIV0 | INVAL | |||
| FMOV | — | — | — | — | — | — | — | — | — |
| FMOVC | — | — | — | — | — | — | — | — | — |
| Status Bit Set/Clear/Update Instructions | |||||||||
| FAND | ⇓ | ⇓ | ⇓ | ⇓ | ⇓ | ⇓ | ⇓ | Logical AND with FSR[15:0] | — |
| FIOR | ⇑ | ⇑ | ⇑ | ⇑ | ⇑ | ⇑ | ⇑ | Logical OR with FSR[15:0] | No exceptions are generated as a consequence of setting an exception flag. |
| FTST | — | — | — | — | — | — | — | — | No result is delivered other than FTST status (FSR[28:24]). |
| Conversion Instructions | |||||||||
| FLI2F | 0 | 0 | ⇕ | 0 | 0 | 0 | 0 | INX: See Generating FP Exceptions | INX: Destination will be written with inexact floating-point result. |
| FDI2F | 0 | 0 | ⇕ | 0 | 0 | 0 | 0 | INX: See Generating FP Exceptions | INX: Destination will be written with inexact floating-point result. |
| FF2LI | ⇕ | ⇕ | ⇕ | 0 | 0 | 0 | ⇕ | HUGI: Result exceeds target register size INX: See Generating FP Exceptions INVAL: ∞, sNaN or qNaN SUBO: Subnormal operand(3) | HUGI: Destination will be written with either most
positive or most negative integer, matching sign of input
operand. HUGI will also cause INVAL to be set. INX: Destination will be written with inexact integer result. INVAL: Destination will be written with integer indefinite value if HUGI is not set, or value defined above if HUGI is set. Assertion of SUBO will not affect integer result. |
| FF2DI | ⇕ | ⇕ | ⇕ | 0 | 0 | 0 | ⇕ | HUGI: Result exceeds target register size INX: See Generating FP Exceptions INVAL: ∞, sNaN or qNaN SUBO: Subnormal operand(3) | HUGI: Destination will be written with either most
positive or most negative integer, matching sign of input
operand. HUGI will also cause INVAL to be set. Note: INX: Destination will be written with inexact
integer result. INVAL: Destination will be written with integer indefinite value if HUGI is not set, or value defined above if HUGI is set. Assertion of SUBO will not affect integer result. |
| Comparison Instructions | |||||||||
| FCPS | ⇕ | 0 | 0 | 0 | 0 | 0 | ⇕ | INVAL: sNaN or qNaN SUBO: Subnormal operand(3) | No result is delivered other than FCPS/FCPQ status (FSR[19:16]). |
| FCPQ | ⇕ | 0 | 0 | 0 | 0 | 0 | ⇕ | INVAL: sNaN SUBO: Subnormal operand(3) | No result is delivered other than FCPS/FCPQ status (GT, LT, EQ or UN). |
| FFLIM | ⇕ | 0 | 0 | 0 | 0 | 0 | ⇕ | INVAL: sNaN SUBO: Subnormal operand(3) | Refer to Table 3-13 for the result delivered. Operand value of -0 compares to less than +0. |
| FMAX | ⇕ | 0 | 0 | 0 | 0 | 0 | ⇕ | INVAL: sNaN SUBO: Subnormal operand(3) | Refer to Table 3-12 for the result delivered. Operand value of -0 compares to less than +0. |
| FMAXNUM | ⇕ | 0 | 0 | 0 | 0 | 0 | ⇕ | INVAL: sNaN SUBO: Subnormal operand(3) | Refer to Table 3-12 for the result delivered. Operand value of -0 compares to less than +0. |
| FMIN | ⇕ | 0 | 0 | 0 | 0 | 0 | ⇕ | INVAL: sNaN SUBO: Subnormal operand(3) | Refer to Table 3-12 for the result delivered. Operand value of -0 compares to less than +0. |
| FMINNUM | ⇕ | 0 | 0 | 0 | 0 | 0 | ⇕ | INVAL: sNaN SUBO: Subnormal operand(3) | Refer to Table 3-12 for the result delivered. Operand value of -0 compares to less than +0. |
| Math Instructions | |||||||||
| FADD | ⇕ | 0 | ⇕ | ⇕ | ⇕ | 0 | ⇕ | INX: See Generating FP Exceptions
UDF: See Generating FP Exceptions OVF: See Generating FP Exceptions INVAL: ((-∞) + ∞) or sNaN SUBO: Subnormal operand(3) | INX: Will also be set if OVF is set. Will also be set if
UDF is set and result is not an exact subnormal. INX/UDF/OVF: Destination will be written with a rounded result. 2 Note: INVAL: Destination will
be written with the distinguished qNaN or quieted
sNaN.1 |
| FSUB | ⇕ | 0 | ⇕ | ⇕ | ⇕ | 0 | ⇕ | INX: See Generating FP Exceptions
UDF: See Generating FP Exceptions OVF: See Generating FP Exceptions INVAL: (∞ - ∞) or sNaN SUBO: Subnormal operand(3) | INX: Will also be set if OVF is set. Will also be set if
UDF is set and result is not an exact subnormal. INX/UDF/OVF: Destination will be written with a rounded result. 2 INVAL: Destination will be written with the distinguished qNaN or quieted sNaN. |
| FNEG | ⇕ | — | — | — | — | — | — | SUBO: Subnormal operand(3) | IEEE-754 requires no result exceptions be signaled. Subnormal operand exception is signaled or SAZ mode applied to ensure result consistency with that of an equivalent sequence of FPU arithmetic instructions. |
| FABS | ⇕ | — | — | — | — | — | — | SUBO: Subnormal operand(3) | IEEE-754 requires no result exceptions be signaled. Subnormal operand exception is signaled (or SAZ mode applied) to ensure result consistency with that of an equivalent sequence of FPU arithmetic instructions. |
| FMUL | ⇕ | 0 | ⇕ | ⇕ | ⇕ | 0 | ⇕ | INX: See Generating FP Exceptions UDF: See Generating FP Exceptions OVF: See Generating FP Exceptions INVAL: (0 * ∞) or (∞ * 0) or sNaN SUBO: Subnormal operand(3) | INX: Will also be set if OVF is set. Will also be set if
UDF is set and result is not an exact subnormal. INX/UDF/OVF: Destination will be written with a rounded result. 2 INVAL: Destination will be written with the distinguished qNaN or quieted sNaN. |
| FMAC | ⇕ | 0 | ⇕ | ⇕ | ⇕ | 0 | ⇕ | INX: See Generating FP Exceptions UDF: See Generating FP Exceptions OVF: See Generating FP Exceptions INVAL: (0 * ∞)+c or (∞ * 0)+c or sNaN SUBO: Subnormal operand(3) | INX: Will also be set if OVF is set. Will also be set if
UDF is set and result is not an exact subnormal. INX/UDF/OVF: Destination will be written with a rounded result. 2 INVAL: Destination will be written with the distinguished qNaN or quieted sNaN.1 INVAL will also be signaled if accumulation is a subtraction of infinities. |
| FDIV | ⇕ | 0 | ⇕ | ⇕ | ⇕ | ⇕ | ⇕ | INX: See Generating FP Exceptions
UDF: See Generating FP Exceptions OVF: See Generating FP Exceptions DIV0: Finite Dividend with Divisor = 0 INVAL: (0/0) or (∞/∞) or sNaN SUBO: Subnormal operand(3) | INX: Will also be set if OVF is set. Will also be set if
UDF is set and the result is not an exact subnormal. INX/UDF/OVF: Destination will be written with a rounded result. 2 DIV0: Result of (±x/±0) will be ±∞ by default, where sign is XOR of operand signs. INVAL: Destination will be written with the distinguished qNaN or quieted sNaN.1 (0/0) or (∞/0) are special cases and will not set DIV0. Result of (∞/0) is correctly signed infinity. Result of (0/0) is the distinguished qNaN with INVAL signaled. |
| FSQRT | ⇕ | 0 | ⇕ | 0 | 0 | 0 | ⇕ | INVAL: x < 0 or sNaN SUBO: Subnormal operand(3) | INVAL: Destination will be written with the
distinguished qNaN or quieted sNaN.(1) FSQRT(±0) = ±0 (no exception signaled) |
| FSIN | ⇕ | 0 | ⇕ | ⇕ | 0 | 0 | ⇕ | INX:See Generating FP Exceptions UDF:See Generating FP Exceptions INVAL: | x | = ∞ or sNaN SUBO: Subnormal operand(3) |
INX: Will also be set if UDF is set and the result is not an exact subnormal. INX/UDF: Destination will be written with a rounded result. (2) INVAL: Destination will be written with the distinguished qNaN or quieted sNaN.(1) |
| FCOS | ⇕ | 0 | ⇕ | ⇕ | 0 | 0 | ⇕ | INVAL: | x | = ∞ or sNaN SUBO: Subnormal operand(3) | INVAL: Destination will be written with the distinguished qNaN or quieted sNaN.(1) |
| Key: ⇕ = set or cleared, ‘0’ = always cleared, — =
unchanged, ⇑ = may be cleared but never set, ⇓ = may be set but never cleared Note:
| |||||||||