2.70.3 NVMCTRL_SetWriteMode Function
C
void NVMCTRL_SetWriteMode(NVMCTRL_WRITEMODE mode);
Summary
Sets the write mode for Flash.
Description
There are four write mode supported. Use this function to set the appropriate write mode, before performing Flash writes. The default write mode is Manual Write.
Precondition
None
Parameters
Param | Description |
---|---|
mode | Enumerated type, indicates one of the four write modes. |
Returns
None.
Example
NVMCTRL_SetWriteMode(NVMCTRL_WMODE_AP);