10.4.12.2 Dual Port RAM for IGLOO®, ProASIC® 3 and Fusion I/O Description

The following table lists the I/O description of a Dual Port RAM for IGLOO, ProASIC3 and Fusion.

Table 10-194. IGLOO, ProASIC3 and Fusion Dual Port RAM I/O Description
NameDirectionDescription
INITADDRINAddress from Flash Memory module
INITDATA[08:00]INData from Flash Memory module
INIT_CLIENT_iINWrite enable signal from the Flash Memory module.This indicates that the data on the INITDATA bus is to be written into the RAM at the INITADDR location. There is a signal per RAM block used. For example, if the memory configuration required 4 RAM blocks, then there are 4 of these signals exported.These signals need to be connected to the<client_name>_block_i_DAT_VAL from the Initialization/Flash Memory module.
INITACTIVEINNeeds to be asserted when Initialization is being performed. Switches the aspect ratio to x9 width and changes the RAM to respond to the Initialization interface.
INITDOUT[08:00]OUTData to be saved into the Flash Memory module.
SAVEACTIVEINNeeds to be asserted when Save is being performed. Switches the aspect ratio to x9 width and changes the RAM to respond to the Save interface.The address location to be read is also driven from the INITADDR port for SAVE operations.